User Activity

The figure is missing: Also, the figure that was there in Rev. 6 referred to DMAMUX_RGCnCR but it should have been DMAMUX_RGxCR.
Various STM32 products have opamps that have a mux in front of it.Ex: STM32G4, STM32F3, STM32H7 series, etc.If I change the mux input setting using the control status register (OPAMPx_CSR::VP_SEL or VN_SEL), how long does it take for the mux to switc...
I use HSI16 as my clock base which goes through a PLL and then into the HRTIM.Let's say that I adjust HSI16 periodically (every ~10 milliseconds) to track an external high precision clock.Is enabling the DLL calibration (HRTIM_DLLCR:CALEN, CALTRE) en...
Figure 188, Page 853: The last waveform (HRTIM_REPxR = 2) should be: 1, 0, 2, 1, 0 and not 1, 0, 2, 0.Figure 254, Page 933: For the last two waveforms (ADCxPSC[4:0]=4 ADROM[1:0]=01 and ADCxPSC[4:0]=4 ADROM[1:0]=10), it seems like the waveforms as sho...
PA9 - Alternate functions has "OMP5_OUT," instead of "COMP5_OUT,"
Kudos from