cancel
Showing results for 
Search instead for 
Did you mean: 

is there any STM32 controller with FPU ? with out changing the hardware i need to replace stm32f030c8t6 with new one with FPU ? .

karthik.b
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5

Double or Single Precision?

Is that a 144-pin device? Guessing not

Floating point is done in software on CM0 and CM3 parts.

The CM4F has a single precision FPU​ that does some basic math functions, the remainder are handled in the library code.

Without some more specific reasoning, it sounds like you need a redesign.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

There aren't any that are pin compatible. There are some that are close but have an additional VDD/VSS pair. See the "Pinout compatible" search feature in CubeMX.

If you feel a post has answered your question, please click "Accept as Solution".
Thanks TDK community
Karthik.B

Thanks you clive1

Thanks TDK