STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! All I want is a LED to blink...

Hello Gals/Guys. I recently purchased a NUCLEO-F439ZI after playing around with F0-DISCOVERY. As is tradition, I wanted to make a LED blink. I have failed miserably. I started in CubeMX to for the initial setup using all the defaults. Using the...

WCook.1 by Associate
  • 4302 Views
  • 4 replies
  • 0 kudos

STM32F4 LINBUS Communication Example

Hello I am working with the STM32f4 development board. I'll make one LIN(Local Interconnet Network) master and one LIN Slave instance but I don't have any example.Has anyone created a sample code?

Resolved! AN4207 Single ended zero reference mode

Hello.Reffering to AN4207(Doc ID 023945 Rev 1) Single ended zero reference mode (Page 9):This mode injects an input common mode of half scale to the ADC thus maintaining the dynamic range the same as in differential mode (-32767 to +32767). In this m...

glinsky by Associate
  • 1873 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F103 timer interrupt fastest time is less than 1us?

I use STM32F103CB in my project.​ but I found timer interrupt fastest time can't less than 1us. Timer prescaler is 0, up counter mode, counter period is 36, no inernal clock division and auto-reload enable. When timer interrupt occur. I set Pin high ...

0693W000007D8VpQAK.jpg

The timer input mode is not working. (using STM32F103RB)

Hi all,I test the timer input capture mode. The input range is 1Hz ~ 100Hz.I set the parameter as below. (Using CUBEMX)Timer Clock : 60MhzPSC : 6000ARR: 10000void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) { HAL_GPIO_WritePin(LED_PORT, IN_...

dKim.1 by Associate II
  • 2048 Views
  • 4 replies
  • 0 kudos

STM32L432KC Nucleo failing to receive serial data from PC

My intention is to program the STM32L432KC to utilize UART2 to monitor incoming serial data from the PC Virtual Com Port via interrupts.void HAL_UART_MspInit(UART_HandleTypeDef* huart) { GPIO_InitTypeDef GPIO_InitStruct = {0};   if(huart->Instanc...

MBenn.2 by Associate
  • 2073 Views
  • 3 replies
  • 0 kudos