STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L412 issues...

I have built many STM32 boards and usually bringing them up is a snap. This time I'm having trouble.... The chip is the 48-pin STM32L412CB. When I boot in DFU mode (it does so by default) I get dfu-util: Error during special command "ERASE_PAGE" get_...

Bug in BSP driver for STM32H743-EVAL onboard LEDs

In case anybody wondered why the red LED of STM32H743-EVAL does not work unless I/O extender is enabled - here is the fix.In this placehttps://github.com/STMicroelectronics/STM32CubeH7/blob/beced99ac090fece04d1e0eb6648b8075e156c6c/Drivers/BSP/STM32H7...

Pavel A. by Super User
  • 1175 Views
  • 1 replies
  • 0 kudos

how can i update firmware over any CAN bus?

Dear Madam/Sir,we are using STM32F4 series microcontroller. ı wonder that how can i update firmware over any CAN bus. Do you have any sample code or tool to do this? Really i dont know how can i do. There is no answer about this issue on internet.

Auysa.1 by Associate
  • 7822 Views
  • 3 replies
  • 1 kudos

System clock configuration using register level program.

We are working on an existing project, in which our microcontroller's flash size was exceeding the value of our code size. So we decided to move to a register level program.We did system clock configuration at 64 MHz, while debugging after step no 3 ...

0693W000008GOVHQA4.png 0693W000008GOL2QAO.png
ATetg.1 by Associate
  • 1998 Views
  • 3 replies
  • 0 kudos

NUCLEO-L476RG: Write ADC values into SD_CARD using SPI

Good Morning. For my thesis work, I have to develop a sensor for seismocardiography based on sensortile. Being unfamiliar with microcontrollers, I'm running some tests using an L476RG nucleo board.I created a project that foresees continuous analog-d...

GChir.2 by Associate II
  • 6908 Views
  • 16 replies
  • 0 kudos