STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't Recieve/Send data to hc-06

my code at below. i can connect succesfull but i cant send any command (like on,off) . what is wrong? help me pls#include "main.h" #include "main.h" #include "stm32f4xx_hal.h" #include "stm32f4xx_hal_uart.h" #include "stm32f4xx_hal_usart.h" #include ...

Aozca.3 by Associate
  • 1490 Views
  • 2 replies
  • 0 kudos

[STM32F0] How to generate PWM with DMA

Hello, I'm working with CubeMX to configure my MCU (STM32F030CCT6TR) for my school project. I want to generate a PWM with DMA but I don't know how to do it even after doing researches.Currently I configure my DMA as attached. Can you help me ?Best re...

JDooe by Associate II
  • 4096 Views
  • 6 replies
  • 1 kudos

Resolved! I want to use DMA for UART receive. How do I generate an interrupt using the HAL for idle line? The UART Callbacks are disabled in the HAL when you use DMA. And it does not look like there is a call back for idle_line in the HAL.

When I setup the UART i activated both DMA TX and RX, and I turned on the UART Interrupt in the MX program. Looking at the code in stm32f4xx_hal_uart.h Around line 680/* Callbacks Register/UnRegister functions ***********************************/#if ...

KiptonM by Lead
  • 1541 Views
  • 1 replies
  • 0 kudos

problem with STM32F411CEUx and HAL on SDIO and ADC.

Hello everyone, first of all I apologize for my English as I am not fluent in it.I am using the STM32F411 and SE and when using two DMAs for Tx and Tx it always shows BUSY in HalState. This I have solved (although not totally yet) by choosing only on...

LLope.1 by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos

Nucleo STM32F091 skips startup script to 'LoopForever'

I've been attempting to debug a test application compiled for an stm32f091RC controller on its corresponding nucleo development board. To debug, I use st-util and arm-none-eabi-gdb. When I load the elf file through gdb, the stm correctly halts just a...

CBlus.1 by Associate
  • 697 Views
  • 0 replies
  • 0 kudos

Availability of STM32F303

Can we expect shortage issue to go away in the near future. Both JLCPCB and Digikey have been having stock issues for months. I'm unable to get the MCU I've designed my project around (F303C[B/C]Tx). Digikey only has the lower flash mem options avail...

DOCon.1 by Senior
  • 2334 Views
  • 5 replies
  • 0 kudos