STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART Rx Threshold or FIFO Full interrupt not triggered

Hi, I created a test project to wake up L562MCU from STOP Mode when UART RxFIFO Threshold reached or full interrupt triggered or USER Button pressed.The project is based on Example project "UART_WakeUpFromStopUsingFIFO" for L562-DK. Test 1: Rx thresh...

Nucleo overcurrent and overheating issue

I am trying to drive inkjet printer cartridge using Nucleo F746ZG board. But at the moment i connect cartridge to the nucleo board, Controller heats up very much and over current LED starts blinking and if i continue connection about 10 Minutes then...

0693W000008wvnXQAQ.png
Cjosh.1 by Associate II
  • 1033 Views
  • 0 replies
  • 0 kudos

STM32L476 SD DATA TIMEOUT problem

I am running into a problem with the SD card driver on the STM32L476. The DATATIMEOUT flag is occasionally set when trying to do a single block read using the DMA. I have set a breakpoint at the DATATIMEOUT flag in the SD IRQ handler. When the break ...

0693W000008wvDeQAI.png

Resolved! Where I can find patch for STM32Cube_FW_F4_V1.25.2 firmware?

Hello,My problem is similar to this one: https://stackoverflow.com/questions/65905606/stm32cubeide-reports-firmware-package-is-missingUnfortunately I cannot find the patch they were talking about (Patch-CubeF4). After going to the following site: htt...

MJaks.2 by Associate
  • 1373 Views
  • 1 replies
  • 0 kudos

Setting core affinity or switching between cores in STM32H757

Hello Team , Setting core affinity or switching between cores in STM32H757,We are in early phase of design and looking to go with STM32H757XI , We are still not sure which thread to be run on which core ( M4 or M7) We are looking to use keil rtx5 CMS...

CMatad by Associate II
  • 1371 Views
  • 4 replies
  • 0 kudos
TPati.2 by Associate
  • 1472 Views
  • 1 replies
  • 1 kudos

Unable to flash STM32H7B3I-DK

I have tried flashing from TouchGFX and also from CUBEIDE. I did manage to run a first trial of example but after the 3rd modification is went black.The lcd remains black. I add a screenshot with the log from TouchGFX . It states failed to erase memo...

0693W000008wstcQAA.png
BHure.1 by Associate III
  • 670 Views
  • 0 replies
  • 0 kudos