cancel
Showing results for 
Search instead for 
Did you mean: 

Can the STM32 Power Shield (LPM01A) be triggered on AND off?

PaulSwanson
Associate III

The X-NUCLEO-LPM01A Power Shield can be triggered by the target device to start acquisition, using the D7 pin. Can it also be triggered to stop acquisition?

Also, my power shield is currently running v1.0.1. The latest version of the firmware is 1.0.6, but there are no release notes about the updated firmware; so I'm not sure if this would make any difference.

Both the user manual and firmware manual say VERY little about the triggering behaviour.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PaulSwanson
Associate III

Bueller?

Anyone had experience with triggering the X-NUCLEO-LPM01A Power Shield?