cancel
Showing results for 
Search instead for 
Did you mean: 

DMA CCR1 CCR2 conflict I can have signal on PB6 or PB7 but not both on one time. by changing CCR1 and CCR2 arrangement. CCR1, CCR1 =signal on PB6 CCR1, CCR2 = signal on PB7 CCR2, CCR2 = signal on PB7 CCR2, CCR1 = signal on PB6

tkor.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
tkor.1
Associate II
#define SAMPLES 100
#include <libmaple/dma.h>
 
dma_tube_config dma_cfg, dma_cfg2;
int val1[SAMPLES];
int val2[SAMPLES];                   // *******************
int amp = 35;
int cnt = 0;
int time_track = 0;
float stp = 6.2831 / SAMPLES;
int ret = 17;
int out1 = PB7; // TIM4_CH2 DMA_CH4 . 
int out2 = PB6; // TIM4_CH1 DMA_CH3 .                     *************************** 
 
timer_dev *dev1 = PIN_MAP[out2].timer_device;   
timer_dev *dev2 = PIN_MAP[out2].timer_device;
 
void timer_conf()
{
// PB7 TIM4_CH2 DMA_CH4
  timer_dma_set_base_addr(dev1, TIMER_DMA_BASE_CCR2);          // CCR1, CCR1 =  PB6
  timer_dma_set_burst_len(dev1, 1);                            // CCR1, CCR2 =  PB7
  timer_dma_enable_req(dev1, PIN_MAP[out1].timer_channel);     //CCR2, CCR2 = PB7
  timer_set_reload(dev1, 102);                                 //CCR2, CCR1 =  PB6
  timer_set_prescaler(dev1, 0);
 
 
  // PB6 TIM4_CH1 DMA_CH3 .                                  *********************
  timer_dma_set_base_addr(dev2, TIMER_DMA_BASE_CCR2);
  timer_dma_set_burst_len(dev2, 1);
  timer_dma_enable_req(dev2, PIN_MAP[out2].timer_channel);
  timer_set_reload(dev2, 102);
  timer_set_prescaler(dev2, 0);
}
void dma_conf()
{
  dma_init(DMA1);
 // PB7 TIM4_CH2 DMA_CH4
  // PB6 TIM4_CH1 DMA_CH3
  dma_cfg.tube_dst = &(dev1->regs.gen->DMAR);                // PB7
  dma_cfg.tube_dst = &(dev2->regs.gen->DMAR);                // PB6********************
  dma_cfg.tube_src = val1;                                   // PB7
  dma_cfg.tube_src = val2;                                   // PB6********************
  dma_cfg.tube_src_size = DMA_SIZE_32BITS;
  dma_cfg.tube_nr_xfers = SAMPLES;
  dma_cfg.tube_flags = DMA_CFG_SRC_INC | DMA_CFG_CIRC;
  
  dma_cfg.tube_req_src = DMA_REQ_SRC_TIM4_CH2;               //PB7
  dma_cfg.tube_req_src = DMA_REQ_SRC_TIM4_CH1;               //PB6 ********************
  dma_cfg.target_data = 0;
  ret = dma_tube_cfg(DMA1, DMA_CH4, &dma_cfg);
  ret = dma_tube_cfg(DMA1, DMA_CH3, &dma_cfg);
}
void dma_start()
{
  // PB7 TIM4_CH2 DMA_CH4
  dma_enable(DMA1, DMA_CH4);
 timer_resume(dev1);
  dma_enable(DMA1, DMA_CH3);
  timer_resume(dev2);
 
}
void init_wave()
{
  int i;
  for (i = 0; i < SAMPLES; i++)
  {
    val1[i] = 50 + amp * sin(stp * i);
    val2[i] = 50 + amp * sin(stp * i);                      //************************
  }
}
void setup() {
  pinMode(out1, PWM);
  pinMode(out2, PWM);
 
 
  timer_conf();
  dma_conf();
  dma_start();
  init_wave();
}
void loop() {
}

waclawek.jan
Super User

What is this, Arduino and 'F103?

I am not familiar with Arduino, but it appears that you want to run two different DMA channels using the same timer's DCR/DMAR registers. This won't work. But why don't you do it in the way it's designed, i.e. using only one DMA channel updating both CCR1 and CCR2 upon a single trigger from Update?

You may want to read out the timer and DMA registers content and check them against the respective chapters in RM, or post them here.

JW

tkor.1
Associate II

I am using arduino IDE and stm32f103, I need 2 outputs from timer # 4, I have one on PB7 to get second I have a problem.

 But why don't you do it in the way it's designed, i.e. using only one DMA channel updating both CCR1 and CCR2 upon a single trigger from Update ? =. This i don't know