User Activity

Hello,Previously when working with NXP MCUs, I was able to inspect MCU registers and memory whilst debugging through a convenient interface built into the IDE.I'm wondering if the STM32Cube ecosystem, or other ST tools, can provide equivalent functio...
Hello,I want to use UART2 on a NUCLEO-L073RZ for printf output but cannotget it to work for the life of me, please help.Context:In this scenario, I need the UART2 output direct from the PA2 / PA3pins on the ST Morpho header (CN10), in other words, no...
The X-NUCLEO-LPM01A Power Shield can be triggered by the target device to start acquisition, using the D7 pin. Can it also be triggered to stop acquisition?Also, my power shield is currently running v1.0.1. The latest version of the firmware is 1.0.6...
I've got a NUCLEO-L073RZ, STM32CubeIDE and CubeMX are installed (locally on Linux).In CubeIDE, I've installed the MCU package for STM32L0 (Help > Manage Embedded Software Packages).I can even see that it has created a "Repository" directory and the S...
The STM32F0Discovery board comes with accompanying example source code, traditionally. However, now, the relevant download page advises that this is all provided by STM32Cube, but it is not. There is NO example code in the STM32CubeMX / IDE for this ...
Kudos from