STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Trying to find best and most reliable way when using the STM32 timers to change the timebase 'on the fly'.

Hi, I've recently retired from being an electronics design engineer for over 40 years. I wanted to have some fun playing around with micros to do some basic control. I have both the Nucleo-F030R8 and STM32F4 Discovery evaluation boards and have bee...

mistert by Associate II
  • 2652 Views
  • 4 replies
  • 0 kudos

Why does my Opamp PGA seem to be 10, not 16?

Hi,I have a board, with STM32f303. It generally works fine, but I am using the opamps and they are causing me trouble. I have set them up to have PGA of 16, and be internally connected to the ADC, and have test points on my board where I can measure ...

0693W000003C1qsQAC.png 0693W000003C1qJQAS.png
DMolo by Senior
  • 6348 Views
  • 16 replies
  • 0 kudos

Resolved! float correctly displayed in debug but not in release.

Dear experts,i try to use the float library with printf or vsnprintf. The option nano has been checked, the -u _printf_float too. The latest version of STM32cubeIDE, the proc is STM32F446RE. The value of floats are correctly displayed in debug but i...

papageno by Associate III
  • 1642 Views
  • 2 replies
  • 0 kudos

About alternate function of STM32F746

Hello,STM32F74xxx Reference manual (RM0385) 6.3.2 I / O pin alternate function multiplexer and mapping has the following description.After reset the multiplexer selection is alternate function 0 (AF0).I think that when AF0 is selected, it will be ass...

[STM32G474] - ADC Error

Hello everyone,I am currently working with the STM32G474QET6.Trying to measure Honeywell pressure sensors whose output voltage ranges from 0V to 3V.The problem is that the measurements have a much greater error than indicated in the data sheet.To rul...

JTánt.1 by Associate II
  • 2390 Views
  • 2 replies
  • 0 kudos

Using ITM printf on STM32H723 Nucleo board

Hi all,I'm tying to use the ITM printf on my STM32H723 Nucleo board in my Keil project without success. I configured the HAL with CubeMX and add the initialization for the SWD_Init(). I enabled tracing in Keil but I do not get any output. I checked:S...

JSchu.5 by Associate II
  • 12471 Views
  • 9 replies
  • 1 kudos

Why Nucleo F746ZG showing LD5 (Over current) on when running simple LED blink code? Also controller heating is more

Hello i am using Nucleo F746ZG board. When i run simple LED blink code with below code its not showing LD5 (Over current) on.#include "mbed.h"   // Blinking rate in milliseconds #define BLINKING_RATE 500ms int main() { // Initialise the digital pin...

Cjosh.1 by Associate II
  • 5766 Views
  • 11 replies
  • 0 kudos