Is there a maximum buffer size For ADC DMA Length is stated as Uint32
Hi
I am doing an ADC DMA sample using HAL_ADC_Start_DMA. Using ADC1
Setup in multimode with 2 channels Rank1 and Rank2. Using STM32H750
I have a buffer Uint16 buffer [131072] setup in RAM_D2
When i set the length in the HAL_ADC_Start_DMA
HAL_ADC_Start_DMA(&hadc1, (uint32_t *)&buffer, 32768 ) This works
HAL_ADC_Start_DMA(&hadc1, (uint32_t *)&buffer, 65536 ) THis does not work it never comes back to get called by the DMA complete. However if I read the status of the DMA is says busy and the DMA counter counts down to 0.
Thanks
Robin