User Activity

Hey!I'm using the STM32G030F6Px, physical Pin 15 is home of PB0, PB1, PB2, PA8. How do you select which GPIO is connected to the pin? This is explained in the reference manual regarding PA11/PA9, set with the PA11_RMP bit in SYSCFG_CFGR1.There is no ...
Here is the firmware, it's very close to something generated from cube.https://github.com/Machine-Hum/Hydroponic/tree/master/fwBlue pillST link V3Arch LinuxWhen the device is initially plugged in, I can...screen /dev/ttyACM1 115200I then see my hello...
After spending some time looking into the R9 I decided to make the switch. I've been developing on the 76 for a while now. I read the migration document and it doesn't look like there are any differences.​Right now I'm having issues with spi and sd c...