STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Second core not booting up

The STM32 dev board I'm working with is the Nucleo H745ZI-Q.This one has two cores, a M7 and a M4.Now when I try to load code onto it, it runs fine the first time I run the debugger.I noticed that when I reconnect the board, the second core doesn't b...

Jvan .10 by Associate III
  • 3535 Views
  • 5 replies
  • 0 kudos

Auto-polling mode with octal memories is not functional.

Hello everyone,I made a custom board for our design, a STM32L4R9VI and an ospi memory MX25UM51245G are integrated on this board. There is a MX25LM51245G on STM32L4R9I-disco board, but it is not in stock, so I chose this 1.8V version MX25UM51245G. The...

Hzhan.2 by Associate II
  • 876 Views
  • 0 replies
  • 0 kudos

STM32H743 - SPI-DMA timing problem with slave select

Hi everyone,I have a problem with a bidirectional SPI communication. I am using the HAL_SPI_TransmitReceive_DMA function for all my communications and my project is loosely based on the STM SPI example. I have now noticed a problem with my communicat...

MGöll.1 by Associate
  • 1740 Views
  • 2 replies
  • 0 kudos

Receive/Transmit UART data using DMA

Hello,I use with:- Nucleo-H743ZI2 -STM32CubeIDE ver 1.6.0-MCU Package ver 1.9.0I made loopback between PB14 & PB15 , the loopback work i checked it without DMA . I try to send data from buffer and get the data using DMA but it is not working.Thank's

IShar.2 by Associate II
  • 1901 Views
  • 4 replies
  • 0 kudos

Would you tell me the condition(Hi/Low/Hiz/PullHigh/PullLow) of all ports of STM32G474 MCU chip when it gets boot mode with boo0 pin of high?

I'm building a new custom PCB with the MCU(STM32G4) chip and needs to get it updated with a new Firmware through UART by main computer. then I HAVE TO CARE all MCU pins so as NOT to make bad effects on other LSI during boot mode. I need to know all t...

TKoya.1 by Associate
  • 1693 Views
  • 3 replies
  • 0 kudos