cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-L476RG 2 Images Configuration SE_APP_GetActiveFwInfo() failure

OAber
Associate II

Hi,

When calling the SE_APP_GetActiveFwInfo function in the UserApp the NUCLEO-L476RG resets every time without any warning or error.

Maybe it has to do something with my linker configuration? There are no problems during compilation.

Linker script:

/*
*****************************************************************************
**
 
**  File        : LinkerScript.ld
**
**  Abstract    : Linker script for STM32L476RGTx Device with
**                1024KByte FLASH, 96KByte RAM
**
**                Set heap size, stack size and stack location according
**                to application requirements.
**
**                Set memory bank area and size if external memory is used.
**
**  Target      : STMicroelectronics STM32
**
**
**  Distribution: The file is distributed as is, without any warranty
**                of any kind.
**
**  (c)Copyright Ac6.
**  You may use this file as-is or modify it according to the needs of your
**  project. Distribution of this file (unmodified or modified) is not
**  permitted. Ac6 permit registered System Workbench for MCU users the
**  rights to distribute the assembled, compiled & linked contents of this
**  file as part of an application binary file, provided that it is built
**  using the System Workbench for MCU toolchain.
**
*****************************************************************************
*/
 
/* Entry Point */
ENTRY(Reset_Handler)
 
/* Highest address of the user mode stack */
_estack = 0x20018000;
 
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x3000;      /* required amount of heap  */
_Min_Stack_Size = 0x800; /* required amount of stack */
 
INCLUDE mapping_fwimg.ld
INCLUDE mapping_sbsfu.ld
 
/* Specific ROM/RAM UserApp definition */
__ICFEDIT_intvec_start__  = __ICFEDIT_SLOT_Active_1_start__    + 0x200;
APPLI_region_ROM_start    = __ICFEDIT_SLOT_Active_1_start__    + VECTOR_SIZE + 0x200;
APPLI_region_ROM_length   = __ICFEDIT_SLOT_Active_1_end__    - APPLI_region_ROM_start + 1;
APPLI_region_RAM_start    = __ICFEDIT_SE_region_RAM_end__ + 1;
APPLI_region_RAM_length    = 0x20018000 - APPLI_region_RAM_start;
 
/* Specify the memory areas */
MEMORY
{
 ISR_VECTOR (rx)   : ORIGIN = __ICFEDIT_intvec_start__, LENGTH = VECTOR_SIZE
 APPLI_region_ROM  : ORIGIN = APPLI_region_ROM_start, LENGTH = APPLI_region_ROM_length
 APPLI_region_RAM  : ORIGIN = APPLI_region_RAM_start, LENGTH = APPLI_region_RAM_length
}
 
/* Define output sections */
SECTIONS
{
  /* The startup code goes first into FLASH */
  .isr_vector :
  {
    . = ALIGN(8);
    KEEP(*(.isr_vector)) /* Startup code */
    FILL(0);
    . = ORIGIN(ISR_VECTOR) + LENGTH(ISR_VECTOR) - 1;
    BYTE(0)
    . = ALIGN(8);
  } >ISR_VECTOR
 
  .SE_IF_Code : {
  KEEP(*se_interface_app.o (.text .text*))
  } >SE_IF_region_ROM
 
  /* The program code and other data goes into FLASH */
  .text :
  {
    . = ALIGN(8);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)
 
    KEEP (*(.init))
    KEEP (*(.fini))
 
    . = ALIGN(8);
    _etext = .;        /* define a global symbols at end of code */
  } >APPLI_region_ROM
 
  /* Constant data goes into FLASH */
  .rodata :
  {
    . = ALIGN(8);
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    . = ALIGN(8);
  } >APPLI_region_ROM
 
  .ARM.extab   :
  {
  . = ALIGN(8);
  *(.ARM.extab* .gnu.linkonce.armextab.*)
  . = ALIGN(8);
  } >APPLI_region_ROM
  .ARM : {
	. = ALIGN(8);
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
	. = ALIGN(8);
  } >APPLI_region_ROM
 
  .preinit_array     :
  {
	. = ALIGN(8);
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array*))
    PROVIDE_HIDDEN (__preinit_array_end = .);
	. = ALIGN(8);
  } >APPLI_region_ROM
 
  .init_array :
  {
	. = ALIGN(8);
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array*))
    PROVIDE_HIDDEN (__init_array_end = .);
	. = ALIGN(8);
  } >APPLI_region_ROM
  .fini_array :
  {
	. = ALIGN(8);
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array*))
    PROVIDE_HIDDEN (__fini_array_end = .);
	. = ALIGN(8);
  } >APPLI_region_ROM
 
  /* used by the startup to initialize data */
  _sidata = LOADADDR(.data);
 
  /* Initialized data sections goes into RAM, load LMA copy after code */
  .data :
  {
    . = ALIGN(8);
    _sdata = .;        /* create a global symbol at data start */
    *(.data)           /* .data sections */
    *(.data*)          /* .data* sections */
 
    . = ALIGN(8);
    _edata = .;        /* define a global symbol at data end */
  } >APPLI_region_RAM AT>APPLI_region_ROM
 
  /* Extra ROM section (last one) to make sure the binary size is a multiple of the AES block size (16 bytes) and L4 flash writing unit (8 bytes)*/
  .align16 :
  {
    . = . + 1;         /* _edata=. is aligned on 8 bytes so could be aligned on 16 bytes: add 1 byte gap */
    . = ALIGN(16) - 1; /* increment the location counter until next 16 bytes aligned address (-1 byte)   */
    BYTE(0);           /* allocate 1 byte (value is 0) to be a multiple of 16 bytes                      */
  } > APPLI_region_ROM
 
  /* Uninitialized data section */
  . = ALIGN(4);
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section */
    _sbss = .;         /* define a global symbol at bss start */
    __bss_start__ = _sbss;
    *(.bss)
    *(.bss*)
    *(COMMON)
 
    . = ALIGN(4);
    _ebss = .;         /* define a global symbol at bss end */
    __bss_end__ = _ebss;
  } >APPLI_region_RAM
 
  /* User_heap_stack section, used to check that there is enough RAM left */
  ._user_heap_stack :
  {
    . = ALIGN(8);
    PROVIDE ( end = . );
    PROVIDE ( _end = . );
    . = . + _Min_Heap_Size;
    . = . + _Min_Stack_Size;
    . = ALIGN(8);
  } >APPLI_region_RAM
 
 
 
  /* Remove information from the standard libraries */
  /DISCARD/ :
  {
    libc.a ( * )
    libm.a ( * )
    libgcc.a ( * )
  }
 
  .ARM.attributes 0 : { *(.ARM.attributes) }
}
 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
OAber
Associate II

mapping_sbsfu.ld:

/*
*****************************************************************************
**
 
**  File        : LinkerScript.ld
**
**  Abstract    : Linker script for STM32L476RGTx Device with
**                1024KByte FLASH, 96KByte RAM
**
**                Set heap size, stack size and stack location according
**                to application requirements.
**
**                Set memory bank area and size if external memory is used.
**
**  Target      : STMicroelectronics STM32
**
**
**  Distribution: The file is distributed as is, without any warranty
**                of any kind.
**
**  (c)Copyright Ac6.
**  You may use this file as-is or modify it according to the needs of your
**  project. Distribution of this file (unmodified or modified) is not
**  permitted. Ac6 permit registered System Workbench for MCU users the
**  rights to distribute the assembled, compiled & linked contents of this
**  file as part of an application binary file, provided that it is built
**  using the System Workbench for MCU toolchain.
**
*****************************************************************************
*/
 
/* SE Code region protected by firewall */
VECTOR_SIZE = 0x200;
__ICFEDIT_SE_Code_region_ROM_start__       = 0x08000000 + VECTOR_SIZE;
__ICFEDIT_SE_CallGate_region_ROM_start__   = __ICFEDIT_SE_Code_region_ROM_start__ + 0x4;
__ICFEDIT_SE_CallGate_region_ROM_end__     = __ICFEDIT_SE_Code_region_ROM_start__ + 0x1FF;
 
/* SE key region protected by firewall */
__ICFEDIT_SE_Key_region_ROM_start__        = __ICFEDIT_SE_CallGate_region_ROM_end__ + 0x1;
__ICFEDIT_SE_Key_region_ROM_end__          = __ICFEDIT_SE_Key_region_ROM_start__ + 0xFF;
 
/* SE Startup: call before enabling firewall*/
__ICFEDIT_SE_Startup_region_ROM_start__    = __ICFEDIT_SE_Key_region_ROM_end__ + 0x1;
__ICFEDIT_SE_Code_nokey_region_ROM_start__ = __ICFEDIT_SE_Startup_region_ROM_start__ + 0x100;
__ICFEDIT_SE_Code_region_ROM_end__         = __ICFEDIT_SE_Startup_region_ROM_start__ + 0x51FF;
 
/* SE IF ROM: used to locate Secure Engine interface code out of firewall */
__ICFEDIT_SE_IF_region_ROM_start__         = __ICFEDIT_SE_Code_region_ROM_end__ + 1;
__ICFEDIT_SE_IF_region_ROM_end__           = __ICFEDIT_SE_IF_region_ROM_start__ + 0x6FF;
 
/* SBSFU Code region */
__ICFEDIT_SB_region_ROM_start__            = __ICFEDIT_SE_IF_region_ROM_end__ + 0x1;
__ICFEDIT_SB_region_ROM_end__              = 0x0800FFFF;
 
SE_Entry_Secure_ROM_Region_Length = __ICFEDIT_SE_CallGate_region_ROM_end__ - __ICFEDIT_SE_CallGate_region_ROM_start__ + 1;
SE_Key_region_ROM_Length          = __ICFEDIT_SE_Key_region_ROM_end__ - __ICFEDIT_SE_Key_region_ROM_start__ + 1;
SE_Startup_region_ROM_Length      = __ICFEDIT_SE_Code_nokey_region_ROM_start__ - __ICFEDIT_SE_Startup_region_ROM_start__ ;
SE_ROM_region_Length              = __ICFEDIT_SE_Code_region_ROM_end__ - __ICFEDIT_SE_Code_nokey_region_ROM_start__ + 1;
SE_IF_region_ROM_Length           = __ICFEDIT_SE_IF_region_ROM_end__ - __ICFEDIT_SE_IF_region_ROM_start__ + 1;
SB_ROM_region_Length              = __ICFEDIT_SB_region_ROM_end__ - __ICFEDIT_SB_region_ROM_start__ + 1;
 
/* RAM section */
/* SE RAM1 region protected by firewall */
/* SE stack is placed 1st in RAM, stack overflow does not write on other RAM area */
__ICFEDIT_SE_region_RAM_start__     = 0x20000000;
__ICFEDIT_SE_region_RAM_stack_top__ = 0x20000400;
__ICFEDIT_SE_region_RAM_end__       = 0x20000FFF;
 
/* SBSFU RAM1 region */
__ICFEDIT_SB_region_RAM_start__     = __ICFEDIT_SE_region_RAM_end__ + 1;
__ICFEDIT_SB_region_RAM_end__       = 0x20017FFF;
 
SE_RAM_region_Length = __ICFEDIT_SE_region_RAM_end__ - __ICFEDIT_SE_region_RAM_stack_top__ + 1;
SB_RAM_region_Length = __ICFEDIT_SB_region_RAM_end__ - __ICFEDIT_SB_region_RAM_start__ + 1;
 
MEMORY
{
 SE_Entry_Secure_ROM_Region (rx)     : ORIGIN = __ICFEDIT_SE_CallGate_region_ROM_start__, LENGTH = SE_Entry_Secure_ROM_Region_Length
 SE_Key_region_ROM (rx)              : ORIGIN = __ICFEDIT_SE_Key_region_ROM_start__, LENGTH = SE_Key_region_ROM_Length
 SE_Startup_region_ROM (rx)          : ORIGIN = __ICFEDIT_SE_Startup_region_ROM_start__, LENGTH = SE_Startup_region_ROM_Length
 SE_ROM_region (rx)                  : ORIGIN = __ICFEDIT_SE_Code_nokey_region_ROM_start__, LENGTH = SE_ROM_region_Length
 SE_IF_region_ROM (rx)               : ORIGIN = __ICFEDIT_SE_IF_region_ROM_start__, LENGTH = SE_IF_region_ROM_Length
 SB_ROM_region (rx)                  : ORIGIN = __ICFEDIT_SB_region_ROM_start__, LENGTH = SB_ROM_region_Length
 SE_RAM_region (xrw)               : ORIGIN = __ICFEDIT_SE_region_RAM_stack_top__, LENGTH = SE_RAM_region_Length
 SB_RAM_region (xrw)               : ORIGIN = __ICFEDIT_SB_region_RAM_start__, LENGTH = SB_RAM_region_Length
}
 

OAber
Associate II

This issue had been resolved, the linker options were in an incorrect order.