STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Implementing the HSE on the STM32G030K6Tx

Hi all,I am designing a PCB using the STM32G030K6Tx and for my application I only require the HSE external crystal, which I believe I connect to GPIO pins PC14 and PC15. When I go the the .ioc file in the STM32CubeIDE (System Core -> RCC) I see there...

MattH2 by Associate III
  • 1471 Views
  • 8 replies
  • 2 kudos

Resolved! STM32G0 ADC Sampling

Configure STM32G0 to sample 11 channels; When voltage is injected into only one channel each time, the sampling values of all channels are correct. When voltage is injected into 11 channels simultaneously, the sampling values of all channels are inco...

Jerry11 by Associate
  • 890 Views
  • 4 replies
  • 0 kudos

Resolved! Bootloader use in-system

Hello,I am beginning development with MCUs, am new to this.  At the moment, I am at the design stage.I have identified a device which seems most suitable for my application, STM32G0B1CET in this case.I am trying to understand the I/O constraints.  I ...

Stefan_S by Associate
  • 509 Views
  • 1 replies
  • 1 kudos

STM32H753VI thermal dissipation calculation

Hi Team, We are performing thermal simulation where the part STM32H753VI included in my board.We are powering STM with 3V3 and we would like to understand the below parameters,1)Tj,2)Thermal simulation data if any3) Efficiency to calculate the power ...

Resolved! STM32F103RET6 bare metal SPI3

I have SPI1 working in bare metal on a 48 pin version of the same chip, but I am having difficulty with SPI3 migrating to a 64 pin.  For reference, I have attached the most recent stm32f103x6.h file from the Cube MX F1 package (STM32Cube_FW_F1_V1.8.0...

joesnyder by Associate III
  • 937 Views
  • 2 replies
  • 2 kudos

how to use stm32f407 dual can communication(can1 & can2)

Hello.I'm currently researching can communication with stm32f407vg​currently, i want to use can1 and can2 at the same time, but only one of them works.​​canfilter is used, and the test is currently in progress through timer interupt.​maybe the can fi...

0693W00000NqK9JQAV.png 0693W00000NqK8gQAF.png 0693W00000NqK9TQAV.png 0693W00000NqK9UQAV.png
KHyun.1 by Associate II
  • 10136 Views
  • 16 replies
  • 1 kudos

STM32H7 ADC Baremetal - Cannot get ADC module ready

I am trying to make baremetal ADC driver for following development board STM32H723ZG Nucleo (144 pins).Reference manual: STM32H723 Reference ManualDatasheet STM32H7xx Nucleo DatasheetTo simplify, lets assume (for example) to use PA3. According to Dat...

AJelen by Associate II
  • 5555 Views
  • 9 replies
  • 1 kudos