User Activity

Board: STM32F407G-DISC1IDE : StmCubeIDEHello,      I am trying to drive ADXL345 accelerometer sensor via SPI. I succeed in receiving the device address (0xE5).However, afterwards, when I tried to read two registers' value consecutively. I always read...
Hello, STM32F407G DISC-1, STMCubeIDE I configured timer3 for generating PWM signal which is 1kHz with %70 duty cycle. I connected its pin(PB4)  to input capture channel(PA1). I use default HSI clock 16Mhz.  I can measure this PWM signal using logic a...
Greetings,                 STMCubeIDE         STM32F407G-DISC1       I am tryiny to read a stable analog signal from LM35 output pin.However, I usually read zeros.The rest of the data also make no sense.Because the data range between each other is ve...
STM32F407G DISC-1   STMCubeIDEGreetings, I am trying to send data to LCD screen by using I2C Communication Protocol. I succeed in doing it by using HAL library. Also, my current work does work in debug mode.However, I could not make it work by runnin...
Hi,   STM407G DISC-1 STMCubeIDEWhen I configure PA6 pin as an input with pull-down. In a floating state, I still measure approximately 2.8V.Do I have to use an external pull-down to make it near to zero?
Kudos from