STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI always calling callback

Hello to everyone. I'm creating a project where i need to communicate via SPI. My main board, is configured as full duplex Master, and i have other STM working as full duplex slave. But, i have a problem. If i configure the boards to just have one fu...

IRodr.2 by Associate II
  • 3373 Views
  • 4 replies
  • 0 kudos

Use HAL_SPI_Receive_DMA receive data. Sometimes the received data shift 3 bytes. Why? The board is STM32F750, build as SPI slave.

SPI slave receives data of unknow size.When SPI master gives a rising edge, SPI slave detects the rising edge and starts HAL_SPI_Receive_DMA(define a large size amount of data to be received). When SPI master gives a falling edge, SPI slave detects t...

Joey.z by Associate
  • 988 Views
  • 1 replies
  • 0 kudos

ADC + DMA convCplt and convHalfCplt

Hi,I am trying to use a circular DMA to transfer ADC samples on STM32L4R9VI.I configured a 3.2 Msps sampling frequency, which means that HAL_ADC_ConvCpltCallback and HAL_ADC_ConvHalfCpltCallback must be called each 10 ms for a 64000 elemets buffer.Ho...

0693W00000BabBbQAJ.png 0693W00000BabBqQAJ.png
ABouk.1 by Associate III
  • 943 Views
  • 1 replies
  • 0 kudos