User Activity

Hello,I have installed and used STM32cubeIDE 1.15.1 on some workstations, and I want to replicate exactly this development environment on a new workstation.In the downloads page, this version 1.15.1 is no longer available for Linux Debian.Where can I...
Hello,I get this compilation warning: The float formatting support is not enabled, check your MCU Settings from "Project Properties > C/C++ Build > Settings > Tool Settings", or add manually "-u _printf_float" in linker flags.The stated "recipe" to f...
Related to the STM32G030xx HAL driver.Many examples of the macro __HAL_FLASH_CLEAR_FLAG use multiple flag values ORed together. The comments on this macro seem to suggest that this is OK since the plural form is used on flagS ("Clear the FLASH pendin...
For whatever reason, I can't delete this post. It is closed, see resolution below.--------------------------Hello. We made a board that powers the VBAT pin of a ​STM32L431RCT6 directly from a coin cell battery. The LSE and RTC work well. But we reali...
When running /opt/st/stm32cubeide_1.8.0/stm32cubeide under Ubuntu 20.04.3 LTS, I get the following NPE when double-clicking on the ioc file. Nothing happens at the UI level. I include the ioc file that makes the program crash in case it could be usef...
Kudos from