STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Alternate blocking and interrupt UART reception

Hello, everyone.I'm working on a project based on an STM32L4 MCU. My project needs to receive some commands asynchronously, to start and stop processing and tune internal parameters. I also need to be able to stream large chunks of data in and out.I'...

Yaxit by Associate II
  • 3042 Views
  • 5 replies
  • 0 kudos

Resolved! AS4C16M16SA external SDRAM with STM32H745 Interface Driver

The STM32H745I-DISCO evaluation board used MT48LC4M32B2 as external SDRAM. But due to unavailability and pricing we had to chooses AS4C16M16SA part. But could not find any reference driver or wrapper for touchgfx for this IC under cube projects.Can a...

YSN by Senior
  • 1913 Views
  • 2 replies
  • 0 kudos

Resolved! ST25RU3993 Migrations

Hi,I am working on the ST25RU3993 UHF eval kit and done the required testing & other feasibility tests accordingly. Now for further development we are facing issue with shorting of STM32L476RGT6, based on searches I have found one replacement STM32G4...

SSing.10 by Associate II
  • 1456 Views
  • 2 replies
  • 0 kudos

Resolved! I'd like to use the same firmware for different types of MCU.

Hello everyone,​​I faced a shortage of MCU materials.So I found an MCU that uses the same pin map.I would like to change STM32F767IIT to STM32F767IGT.​Please let me know if the change is okay.Clock does not work when using STM32F767IGT. If...

hjuns by Associate III
  • 1814 Views
  • 3 replies
  • 0 kudos

Resolved! Range of temperature using NUCELO-F439

Hello,I am using right away a Nucle-144 smt32f439ZI for a specific development. I have red in the datasheet, the µC can be used in a temperature range of -[40, +105°]. But I didn't see anywhere the same characteristics for Nucleo-144. Any idea? Than...

LBadi.1 by Associate II
  • 1629 Views
  • 2 replies
  • 0 kudos

Transfer from STM32f411RE to STM32F411ce

Hi there,Recently if done a project regarding custom hid on a STM32F411RE Nucleo prototype board, this was successful. I have created my own pcb design but unfortunatly due the lack of availability of the STM32F411RE i was forced to go with the STM32...

MHovi.1 by Associate II
  • 5574 Views
  • 15 replies
  • 0 kudos