STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Timing parameter confusion

I'm interfacing a camera module (OV2640) with STM32F446RE. I've found a driver on github for this camera however the given example from the github repository is for an F7 chip. I've integrated all the files for my f446re chip and everything runs corr...

0693W00000D0YK7QAN.jpg
ZHama.1 by Associate II
  • 2452 Views
  • 7 replies
  • 0 kudos

Resolved! Is any System Flash writable?

I am using an STM32H743ZI processor and I am confused by an ambiguity in the manual (RM0433). On page 152, the lower table shows two banks of System Flash, bank 1 is 0x1FF00000-0x1FF1FFFF and bank 2 is 0x1FF40000-0x1FF5FFFF. Only bank 1 is marked as ...

JLesser by Associate
  • 1380 Views
  • 1 replies
  • 0 kudos

Timer interrupt stm32f103c8

How can I make PC 13 blink at a time I set using any timer in stm32f103 using interrupt (without hal library) ?

Bicer by Associate II
  • 3580 Views
  • 4 replies
  • 0 kudos

TIM1 doesnot enter CC interrupt

hello dear forum,my 103c8 blue pill doesnot enter TIM1 CC interrupt although there is square wave at A8 pinthe variable which I increment inside interrupt routine doesnot count I can see TIM1 counting in CubeIDE I am missing something but I cant f...

0693W00000D0WDdQAN.png

Resolved! Out of range channel written in ADC seq register for STM32L475

Hi,What happens if I write them out of range channel numbers in the ADC sequence register.For STM32L475, the channel range is 0 -18 but I wrote the channel number 19. While debugging, from debug window I found that the seq. register accepting number ...

Harish1 by Associate III
  • 796 Views
  • 1 replies
  • 0 kudos

FSMC - Multiplexed vs Non-Multiplexed mode on LQFP100 packages

I have used the FMC successfully in several projects to memory-map certain devices in a Non-Multiplexed mode where separate data and address lines are assigned. On devices with smaller package (e.g., STM32F407) the FSMC is only available in multiplex...

Zaher by Senior II
  • 2938 Views
  • 4 replies
  • 0 kudos