STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [Solved]Writing external SRAM cause Hardfault - 32L496GDiscovery

By learning from example STM32Cube_FW_L4_V1.15.1\Projects\32L496GDISCOVERY\Examples\FMC\FMC_SRAM, I tried to setup a simple SRAM program in STM32CubeIDE 1.7.0.​When I was asked if I want to init peripheral or not , I select YES. Then I changed Clock ...

Lsy.1 by Associate II
  • 2609 Views
  • 1 replies
  • 1 kudos

Concerning the RTC peripheral: Can I convert SubSecond Register value to millisecond during a Shift Operation (SHFP=1) ?

RM440 Rev 5 says : "SS can be larger than PREDIV_S only after a shift operation. In that case, the correct time/date is one second less than as indicated by RTC_TR/RTC_DR"Low Layer Driver documentation says: "==> Seconds fraction ratio * time_unit= ...

Pierre.A by Associate II
  • 651 Views
  • 0 replies
  • 0 kudos

Resolved! Internal Command Error STM32F303RE

I'm having this problem when I'm trying to upload my code to the microcontroller. I'm using the STM32F303RE Nucleo board, and whenever I try to upload the code it happens this error: Internal command errorAnd after that, it doesn't let me upload any ...

Hello, Is there any way speed up clock out frequiencies MCK and CK while keeping WS clock out frequency constant at I2S communication(STM32f446)?

My main concern to speed up double MCK and CK clocks frequency while keeping WS frequency constant at the I2S communication. But when i double up the I2S frequency all of the frequencies doubles up. For e.g.;When WS is 43.71kHz, CK = 1.4MHz and MCK =...

MEDİZ.1 by Associate II
  • 2470 Views
  • 3 replies
  • 0 kudos

Trigger I2C DMA RX transfer with LPTIM1 at each (1/200)s

Hi,What I want is mostly in the title, but I'm confused on how to configure LPTIM1.This is the STM32CubeIDE config of LPTIM1 :1) I'm not sure I understand why I can't set the autoreload value (which the reference manual states is a 16-bit register) i...

0693W00000D0vwJQAR.png
YB.1 by Associate
  • 914 Views
  • 0 replies
  • 0 kudos

Pending and disabling of interrupts in STM32L431RCT6

I am using tim6 with a period of 140 ms. In another interrupt that has a priority greater than tim6, I am disabling the tim6 interrupt. But sometimes even after disabling that interrupt, tim6 update interrupt occurs and after that, a variable is corr...

STeja.1 by Associate II
  • 3417 Views
  • 6 replies
  • 0 kudos

Resolved! Resonator on STM32 board design failed...Or maybe not the design? Did I miss something? Help is needed::::::SOLVED!!!!!!!!!!

Hello everyone,I designed my own board which partly failed.I used 32768 Hz ceramic crystal for LSE and 8MHz ceramic resonator for HSE.I can upload my code successfully, but, it doesn't execute unless I disable both LSE and HSE.I'm not professional de...

TAlle.1 by Associate II
  • 5899 Views
  • 3 replies
  • 0 kudos