Skip to main content
Hans T
Associate III
March 27, 2021
Solved

STM32H7 STM32H755iit CM7 ERROR region 'RAM' overlowed by 139396 bytes

ERROR CM7 region 'RAM' overlowed by 139396 bytes

Compiler indicates that there is not enough memory. however the H7-CM7 has 512k, What's wrong?

STM32H755iit STM32H7

STM32CubeMX - STM32 Device Configuration Tool

Version: 6.2.0-RC3 Build: 20210219-1602 (UTC)

STM32Cube FW_H7 V1.9.0

STM32CubeIDE - C/C++ Embedded Development Tools for MCU

Version: 1.6.0.202101291314

c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: RSF3_CM7.elf section `.bss' will not fit in region `RAM'

c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: region `RAM' overflowed by 139396 bytes

/*

******************************************************************************

**

** File    : LinkerScript.ld

**

** Author   : STM32CubeIDE

**

** Abstract  : Linker script for STM32H7 series

**           2048Kbytes FLASH

**           512Kbytes RAM

**

**        Set heap size, stack size and stack location according

**        to application requirements.

**

**        Set memory bank area and size if external memory is used.

**

** Target   : STMicroelectronics STM32

**

** Distribution: The file is distributed as is without any warranty

**        of any kind.

**

*****************************************************************************

** @attention

**

** <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.

** All rights reserved.</center></h2>

**

** This software component is licensed by ST under BSD 3-Clause license,

** the "License"; You may not use this file except in compliance with the

** License. You may obtain a copy of the License at:

**            opensource.org/licenses/BSD-3-Clause

**

*****************************************************************************

*/

/* Entry Point */

ENTRY(Reset_Handler)

/* Highest address of the user mode stack */

_estack = ORIGIN(RAM) + LENGTH(RAM); /*end of "RAM" Ram type memory */

_Min_Heap_Size = 0x200 ; /* required amount of heap */

_Min_Stack_Size = 0x400 ; /* required amount of stack */

/* Memories definition */

MEMORY

{

  RAM  (xrw)  : ORIGIN = 0x24000000, LENGTH = 256K  /* Memory is divided. Actual start is 0x24000000 and actual length is 512K */

 FLASH  (rx)  : ORIGIN = 0x08000000, LENGTH = 1024K  /* Memory is divided. Actual start is 0x8000000 and actual length is 2048K */

 DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K

 RAM_D2 (xrw)  : ORIGIN = 0x30000000, LENGTH = 288K

 RAM_D3 (xrw)  : ORIGIN = 0x38000000, LENGTH = 64K

 ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K

}

/* Sections */

SECTIONS

{

 /* The startup code into "FLASH" Rom type memory */

 .isr_vector :

 {

  . = ALIGN(4);

  KEEP(*(.isr_vector)) /* Startup code */

  . = ALIGN(4);

 } >FLASH

 /* The program code and other data into "FLASH" Rom type memory */

 .text :

 {

  . = ALIGN(4);

  *(.text)      /* .text sections (code) */

  *(.text*)     /* .text* sections (code) */

  *(.glue_7)     /* glue arm to thumb code */

  *(.glue_7t)    /* glue thumb to arm code */

  *(.eh_frame)

  KEEP (*(.init))

  KEEP (*(.fini))

  . = ALIGN(4);

  _etext = .;    /* define a global symbols at end of code */

 } >FLASH

 /* Constant data into "FLASH" Rom type memory */

 .rodata :

 {

  . = ALIGN(4);

  *(.rodata)     /* .rodata sections (constants, strings, etc.) */

  *(.rodata*)    /* .rodata* sections (constants, strings, etc.) */

  . = ALIGN(4);

 } >FLASH

 .ARM.extab  : { 

  . = ALIGN(4);

  *(.ARM.extab* .gnu.linkonce.armextab.*)

  . = ALIGN(4);

 } >FLASH

  

 .ARM : {

  . = ALIGN(4);

  __exidx_start = .;

  *(.ARM.exidx*)

  __exidx_end = .;

  . = ALIGN(4);

 } >FLASH

 .preinit_array :

 {

  . = ALIGN(4);

  PROVIDE_HIDDEN (__preinit_array_start = .);

  KEEP (*(.preinit_array*))

  PROVIDE_HIDDEN (__preinit_array_end = .);

  . = ALIGN(4);

 } >FLASH

  

 .init_array :

 {

  . = ALIGN(4);

  PROVIDE_HIDDEN (__init_array_start = .);

  KEEP (*(SORT(.init_array.*)))

  KEEP (*(.init_array*))

  PROVIDE_HIDDEN (__init_array_end = .);

  . = ALIGN(4);

 } >FLASH

  

 .fini_array :

 {

  . = ALIGN(4);

  PROVIDE_HIDDEN (__fini_array_start = .);

  KEEP (*(SORT(.fini_array.*)))

  KEEP (*(.fini_array*))

  PROVIDE_HIDDEN (__fini_array_end = .);

  . = ALIGN(4);

 } >FLASH

 /* Used by the startup to initialize data */

 _sidata = LOADADDR(.data);

 /* Initialized data sections into "RAM" Ram type memory */

 .data : 

 {

  . = ALIGN(4);

  _sdata = .;    /* create a global symbol at data start */

  *(.data)      /* .data sections */

  *(.data*)     /* .data* sections */

  *(.RamFunc)    /* .RamFunc sections */

  *(.RamFunc*)    /* .RamFunc* sections */

  . = ALIGN(4);

  _edata = .;    /* define a global symbol at data end */

 } >RAM AT> FLASH

 /* Uninitialized data section into "RAM" Ram type memory */

 . = ALIGN(4);

 .bss :

 {

  /* This is used by the startup in order to initialize the .bss section */

  _sbss = .;     /* define a global symbol at bss start */

  __bss_start__ = _sbss;

  *(.bss)

  *(.bss*)

  *(COMMON)

  . = ALIGN(4);

  _ebss = .;     /* define a global symbol at bss end */

  __bss_end__ = _ebss;

 } >RAM

 /* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */

 ._user_heap_stack :

 {

  . = ALIGN(4);

  PROVIDE ( end = . );

  PROVIDE ( _end = . );

  . = . + _Min_Heap_Size;

  . = . + _Min_Stack_Size;

  . = ALIGN(4);

 } >RAM

 /* Remove information from the compiler libraries */

 /DISCARD/ :

 {

  libc.a ( * )

  libm.a ( * )

  libgcc.a ( * )

 }

 .ARM.attributes 0 : { *(.ARM.attributes) }

}

This topic has been closed for replies.
Hans T
Hans TBest answer
Associate III
March 27, 2021

Thanks,

I have change the LinkerScript.ld to 512K

Everything works fine :)

Maybe an idea to set that default to 512K in CubeMx generated code, or add a user setting

RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K /* Memory is divided. Actual start is 0x24000000 and actual length is 512K */

3 replies

MM..1
Super User
March 27, 2021

I dont see your question simply your RAM have 256K and code use more. You need rewrite code to use too other ram parts or change this definition

 RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 256K /* Memory is divided. Actual start is 0x24000000 and actual length is 512K */
  FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K /* Memory is divided. Actual start is 0x8000000 and actual length is 2048K */
  DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
  RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
  RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
  ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K

Tesla DeLorean
Guru
March 27, 2021

Perhaps approach the problem by looking at what is consuming the memory.

Large static allocations? Can they be directed into other RAM regions or folded.

You could expand the RAM size in the Linker Script so that the Linker can get closure and generate a .MAP file for review/analysis

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Hans T
Hans TAuthorBest answer
Associate III
March 27, 2021

Thanks,

I have change the LinkerScript.ld to 512K

Everything works fine :)

Maybe an idea to set that default to 512K in CubeMx generated code, or add a user setting

RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K /* Memory is divided. Actual start is 0x24000000 and actual length is 512K */