STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Two STM32L4 board I2C communication issue, Slave sending the data but master not receiving. can i transmit data from slave to master using this function ? HAL_I2C_Slave_Transmit(&hi2c3, (uint8_t *)Data, strlen(Data), I2C_TIMEOUT);

I have Configured one STM32 board as Master and another is a Slave . When the master send the data slave receiving its fine but when slave sends the data Master not receiving, Acknowledge i am not getting from the Slave when i use HAL_I2C_STATE_READY...

Ssiva.2 by Associate II
  • 4199 Views
  • 5 replies
  • 0 kudos

Resolved! Suspecting document mistake in RM of STM32L475

In the attached image showing the description of the reference manual of stm32L475. Here, it is showing the EOC flag is set to clear by the SW. We can clear the flag but how can SW set the EOC flag. I am suspecting this as a bug in the document. Can ...

0693W00000D0ZdFQAV.png
Harish1 by Associate III
  • 1873 Views
  • 3 replies
  • 0 kudos

Resolved! I2C found the wrong address (Actually 1 shifter version)

Hello Folks,I was doing my I2C example, and I realize that the STM board found an address with one left-shifted.I set my Arduino address as 70 -> 0x46 for hexadecimalvoid setup() { Wire.begin(0x46); // Wire communication begin }I connect my STM32F4...

0693W00000D0pIDQAZ.jpg
SKAŞ.1 by Associate II
  • 2467 Views
  • 3 replies
  • 0 kudos

Configuring HSE using CubeIDE on STM32H750

Using an STM32H750 part, I've lived with the slack tolerance of the HSI until coming to the UART where a speed of 9000 bps is experienced from a configured 9600 bps. This is too far out to be of any use at all and therefore have decided to put on an ...

NSR by Associate III
  • 1219 Views
  • 0 replies
  • 0 kudos

Resolved! Weird data word size in OLED SPI

Hi!I'm using EA W162-XBLG OLED in SPI mode. Timing shown in datasheet is really weird. In instruction diagram there is 20 clock cycles, in data transmission 18. I try to get it to work with STM32F407VG, but I can only set 8 or 16 clock cycles. Maybe ...

0693W00000D0pBvQAJ.png
bmak by Senior
  • 1278 Views
  • 3 replies
  • 0 kudos