Since I am using the version v2.7.0, I get this error after programming both cores after the first time:I can fix this by Disconnecting the STM32H7, and Connected again
ERROR CM7 region 'RAM' overlowed by 139396 bytes Compiler indicates that there is not enough memory. however the H7-CM7 has 512k, What's wrong?STM32H755iit STM32H7STM32CubeMX - STM32 Device Configuration ToolVersion: 6.2.0-RC3 Build: 20210219-1602 (U...
Hello,I'am use the STM32CubeProgrammer v2.60In the USB programming mode, I cannot load DFU files.Is it possible that this option is added, and a possibility to create DFU files ?Thanks Hans
To update users' STM32 chip, a simple DFU program is very useful.Or an example of a C# program environment, so that you can write an Update program yourself
DFU application was an easy way to perform update by a customer who has no knowledge of all kinds of programming programs.I don't have a program yet to update a dual core ARM from SD card.so, I miss an compact and easy DFU tool.It would be useful for...
Thanks,I have change the LinkerScript.ld to 512KEverything works fine Maybe an idea to set that default to 512K in CubeMx generated code, or add a user settingRAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K /* Memory is divided. Actual start is 0...