STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Static Code Analysis Tools For C

Hi everyone,I need a tool for static code analysis to my project. I want to find out your preferences about these tools. C language was used on my project. So I need a tool according to this language. Also I tried to used to PC-Lint tool but I could ...

STM32L151CBU UART 8E1 (Parity) Problem

Hello everyone,I have created a project with STM32L151CBU and used UART2 (PA2, PA3) for communication with some other transceiver IC.I have configured my UART as follows for (1-bit start, 8 bits data, 1 bit EVEN parity, and 1 bit stop) communication....

Resolved! Having trouble with ADC sequencing STM32H7

Hi everyone, hope everyone is doing wellI am trying to setup the STM32H743ZI's ADC for a 5 channel Continuous scan. The 5 scans will be used forThe Input voltage - Channel 0The Input Current - Channel 1The output Voltage - Chanel 2The output Current ...

CLeo.1 by Senior II
  • 5827 Views
  • 13 replies
  • 0 kudos

Troubles enabling the 32.786kHz RTC clock.

Hi all,I am working with a Nucleo STM32L452RE board and I had a bit of trouble enabling the RTC clock. I am just trying to get a scope shot of the waveform output by the clock itself and I noticed it was not on by default. I attempted to use a few ex...

KMill.3 by Associate II
  • 4084 Views
  • 3 replies
  • 0 kudos

32F413: Can I Remove Power from VDDA Pin During Shutdown?

I am chasing reason the for last 4 mA of current that my 32F413 microcontroller draws during low current shutdown. By "shutdown" I mean sleep mode where my system is powered from a small battery with short life.A really good engineer would have equi...

JOlso.12 by Associate III
  • 1354 Views
  • 1 replies
  • 0 kudos