cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am using stm32f407vgt6 that supports fsmc, I need to extend the RAM; is it possible to interface hyperbus RAM chips using the FSMC? if not what are the possible alternatives? kinly note stm32f407vgt does not support QSPI.

JAbde.1
Associate

Hyperbus RAMs requires 12 pins for implementation and offer decent speed. I have already 16 spare pins for the data/address and 10 other pins for fsmc handshaking.

have any one tested this option before? is this easily implemented using HAL library or a custom driver will do it?

I could not find documentation or use cases on the subject if you have please share.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0