STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about calculating i2c timing

I use stm32373c_eval board and I try to acquire and send test data by i2c communication.The max speed of usb-i2c i use is 400k and board i2c clock frequency is 72M.I downloaded the I2C_Timing_Configuration_V1.0.1.xls from st website.I try to configur...

0693W00000GXoyQQAT.png
KShen.1 by Associate II
  • 3515 Views
  • 5 replies
  • 0 kudos

Wake from standby not working. STM32H743IIT6

I have a custom board with an led on PD7 and Normally High push button on PI11. There is also a pushbutton set up on NRST. Device is a  STM32H743IIT6I can get the processor to go into standby okay. This is confirmed by the __HAL_PWR_GET_FLAG(PWR_FLAG...

FColl.1 by Associate III
  • 2164 Views
  • 3 replies
  • 0 kudos

DRDY pin for HTS221 on B-U585I-IOT02A?

Having previously worked with the STM32L4S5 IOT board with an HTS221 on it, I'm familiar with the I2C interface and the HTS221's DRDY exti pin.In the reference manual for the STM32U585-based IOT board, though, there is a giant blank on the I/O line f...

0693W00000GYUd0QAH.png

LSE clock not starting - STM32F373

Hi!I have a STM32F373VBT MCU and I have issues with LSE.First I have selected this crystal.Because STM32 documention recomended it for my processor. Also I notice that I need to have high drive for my crystal because it has a 12.5 pF load capacitance...

0693W00000GY662QAD.png 0693W00000GY66WQAT.png 0693W00000GY68mQAD.png 0693W00000GY5p2QAD.png
DMårt by Lead
  • 4884 Views
  • 9 replies
  • 0 kudos

J link plus programming STm32F46

Hi forum ,we decided to make a test buying a segger j link plus debug probe. We are using SWD debug interfaceWe are using STCubeIde for programming When w etry to program the micro we got : - Can not attach to CPU. Trying connect under reset. - Conne...

SGasp.1 by Senior
  • 1271 Views
  • 2 replies
  • 0 kudos

STM32L151CBT6 as slave with startup and operational phase

Setup:Master: PLD, SPI Frequency 4MHzSlave: STM32L151CBT6, SysClk 32MHzUsing HALConfigured SPI to use DMAWhat I want: Start-Up Phase and Operational Phase for the slave deviceStart-Up Phase:1) The PLD waits untill the uC complete its start up phase a...

Chrizzly by Associate III
  • 1451 Views
  • 2 replies
  • 0 kudos

STMF103C8Tx and VL53L0X ToF sensor

Hello, I'm trying to program and get some readings from VL53L0X sensor with STM32F1C8Tx board and I can't find any examples or guides how to deal with it, because as I understand I need to use API for configuration. Does anyone has did some proje...

DSimp.1 by Associate III
  • 1665 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 corrupt program counter already in Reset_Handler

Hello All,I use the STM32H743ZI MCUs on self designed boards. Most boards run without problems with the developed firmware. But some boards ( -were ok before- ) suddenly show a strange behavior. The STM32H7 seems to reset continuously at first sight....

Ekowa.2 by Associate II
  • 12483 Views
  • 10 replies
  • 0 kudos