STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use Analog Watchdog with DMA on NUCLEO-L476RG?

Hi folks,I want to start ADC conversions on 2 regular channels of ADC1 block only after the voltage on one of the channels exceeds a certain limit, hence I'm using a watchdog feature.After the watchdog will be triggered, I need to store 5 consequent ...

PIvan.9 by Associate II
  • 2222 Views
  • 2 replies
  • 0 kudos

Midi over SPI on STM32F030

I started a project with MIDI, using the SPI peripheral of a STM32F030. I'm no longer sure I can get this peripheral to do what I need it to. I'm using STM32cubeIDE with the setup through the pinout configuration. Midi signals are split into three by...

deep_rune by Associate III
  • 2058 Views
  • 2 replies
  • 0 kudos

Resolved! Need more information on FDCAN

Hi ST members,sorry to say this but FDCAN documentation is not the best part at least in RM0433.I found some more clarity in AN5348 but still can't get ahead.There are these lines in AN5348, page 18:Up to 32 elements are supported by the FDCAN. Each ...

Resolved! Laser sensor tw10sp not working correctly

hello everyone, am working with the laser sensor tw10sp to mesure distance and interfacing it with UART. It require commands to work. i send the HEX command via UART and it response always with the same HEX number (clearly something wrong).Any help p...

0693W00000HqB96QAF.png
Mbhir.1 by Associate II
  • 1613 Views
  • 2 replies
  • 0 kudos

STM32 External HSE crystal not working

STM32 model : STM32F413CGU625MHz crystal : https://media.digikey.com/pdf/Data%20Sheets/AVX%20PDFs/CX3225GA_Series_Spec.pdfThe problem is that I can not connect STM32 by STM32 Cube Programmer. The programmer can not detect STM32 unless I desolder the ...

0693W00000HqMVDQA3.png 0693W00000HqMVXQA3.png
jas.1 by Associate
  • 1972 Views
  • 2 replies
  • 0 kudos