Skip to main content
HWidj.2
Associate II
August 15, 2021
Solved

Bootloader information discrepancy

  • August 15, 2021
  • 2 replies
  • 797 views

Reference Manual for STM32H72xxx/73xxx (RM0468), section 2.6, says that the embedded bootloader can be accessed via I2C1, I2C2, I2C3, I2C4 and SPI1, SPI2, SPI3, SPI4, however AN2606 only lists I2C1, I2C2, I2C3 and SPI, SPI3 as the working I2C and SPI interfaces used.

I didn't notice any discrepancy with the other interfaces.

Can someone help to clarify?

This topic has been closed for replies.
Best answer by Imen.D

Hello @HWidj.2​ ,

AN2606 is correct.

For STM32H72xx/3xx, the bootloader have I2C1/I2C2/I2C3 and SPI1/SPI3/SPI4 (no SPI2).

Thank you for noticing that. The RM0468 will be fixed in the coming releases.

When your question is answered, please close this topic by choosing Select as Best.  This will help other members of the community find this response more quickly. :)

Imen

2 replies

Imen.DBest answer
ST Technical Moderator
August 17, 2021

Hello @HWidj.2​ ,

AN2606 is correct.

For STM32H72xx/3xx, the bootloader have I2C1/I2C2/I2C3 and SPI1/SPI3/SPI4 (no SPI2).

Thank you for noticing that. The RM0468 will be fixed in the coming releases.

When your question is answered, please close this topic by choosing Select as Best.  This will help other members of the community find this response more quickly. :)

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
HWidj.2
HWidj.2Author
Associate II
August 17, 2021

Thanks for the clarification.