STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Enabling MCLK on SAI2 (STM32H745I-DISCO)

I am posting this more as an open question, and perhaps to help someone else...When configuring SAI2 for Audio in CubeMX I had some issues which stemmed from MCLK not appearing to work correctly for the Audio Codec. This would cause the wm8994 to bec...

SNort.1 by Associate II
  • 1719 Views
  • 2 replies
  • 0 kudos

UART Not receive after some hour ,the EIE bit which normally must be at 1 when the UART does not work ,I find it at 0

Dear all,This is my first time using UART, sorry if the question is not relevant.I configured through the Device Configuration Tool the initial code for a STM32H745, in which I use the UART 1 with interrupt.Everything works fine for several hours, ev...

DFont.1 by Associate
  • 2159 Views
  • 3 replies
  • 0 kudos

Resolved! ram_d1 overflowe ?

Hello,I use stm32h750vbt6, I got the ram_d1 zone overflow error.What I don't understand is why the ram_d1 region zone overflow doesn't write to other ram regions.

0693W00000HqWUAQA3.png

Resolved! How to use Analog Watchdog with DMA on NUCLEO-L476RG?

Hi folks,I want to start ADC conversions on 2 regular channels of ADC1 block only after the voltage on one of the channels exceeds a certain limit, hence I'm using a watchdog feature.After the watchdog will be triggered, I need to store 5 consequent ...

PIvan.9 by Associate II
  • 2215 Views
  • 2 replies
  • 0 kudos