STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hey i want to read a temperature sensor and a humidity sensor i want to send the values via cdc to my pc and then read them in c# windows forms my question is now how can i read two adc at the same time so i have separate data ? here you have my stm code

 while (1) {  /* USER CODE END WHILE */  /* USER CODE BEGIN 3 */   HAL_ADC_Start(&hadc2);   HAL_ADC_Start(&hadc1); if (HAL_ADC_PollForConversion(&hadc2, 10) == HAL_OK) {  adcValTemp = HAL_ADC_GetValue(&hadc2);  // Temperature Calculation  adcTem...

MSchmutz by Associate II
  • 2623 Views
  • 4 replies
  • 0 kudos

Resolved! f373 SDADC one input is pulling down.

Hello, I have a custom designed board with 7 analog inputs on sigma delta ADC's.6 of my inputs are working properly. I have a software issue.When I erase the flash or de-solder the mcu I can measure the correct voltage from my test points.But when I ...

Resolved! stm32H723 (nucleo) with SDMMC, FR_NOT_READY

I'm stock since a while now.I use H723 nucleo board with a SD card socket, build for SPI, but I use it as SDMMC with 1bit wide.this socket is ok with SD and SPI.f_mount send FR_NOT_READY.I have the same answer with or with out Sd card...I use a logic...

Tbill.1 by Associate II
  • 2090 Views
  • 1 replies
  • 0 kudos

STM32L4 - ADC Mulit Channel Interrupt support

Hey Guys,I am working with the STM32L476RG Nucleo board (however my custom board has the L462 chip - I am hoping the solution will work for both chips) and I am trying to get multiple channels ADC interrupts to work without success. My CubeMX setup i...

0693W00000Hr00oQAB.png
ASter.2 by Associate II
  • 3277 Views
  • 6 replies
  • 0 kudos

how to adjust the programmer for a different pin out ?

I have a custom board with stm32L496ZG similar to stm32L496G-disco evaluation board.only the CLK and CS for quad spi are different. I want to use the programmer to check the functionality of the external flash that is connected with quad spi. I have ...

Eblec.1 by Associate II
  • 1184 Views
  • 2 replies
  • 0 kudos

G4 HRTIM configuration problem

Hi,I'm currently using HRTIM on a STM32G474RE and I'm facing a configuration problem.Context :The HRTIM is used to produce 2 push-pull PWM outputs from Timer A. The 2 outputs are configured the same way :1 Set source : Timer period event2 Reset sourc...

0693W00000Hpkm1QAB.png 0693W00000HpklcQAB.png
CJARD.1 by Associate
  • 1680 Views
  • 1 replies
  • 0 kudos