STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, I am new to STM32 and I am trying to generate PWM signal of 10 KHZ and 50% duty cycle and i am not able to achive it and I am using STM32L476VG DISCO board and for reference I have attached the code. Thank you

/*CODE to generate PWM signal of 50%*/#include "stm32l476xx.h"#include "pwm.h"void pwm_init(void){ /*RCC configuration*/ RCC->AHB2ENR|=RCC_AHB2ENR_GPIOEEN;//ENABLE GPIOE RCC->APB2ENR|=RCC_APB2ENR_TIM1EN;// ENABLE CLOCK ACCESS TO TIM1 //RCC->APB1ENR1|...

PKuma.23 by Associate II
  • 2245 Views
  • 5 replies
  • 0 kudos

DMA stay in busy state when using HAL_I2C_Slave_Receive_DMA

Hello,I'm working on 2 NUCLEO-F767ZI Demo Board.I'm using STM32CubeMX with last firmware package to generate the code and STM32CubeIDE to modify it and debug it.One of the board is used as an I2C Master, the other as I2C Slave. Every thing work fine ...

ANauz.1 by Senior II
  • 2217 Views
  • 2 replies
  • 0 kudos

Resolved! I need to use PG10-NRST as a GPIO. So I check the Reference manual to find out how to do it. I find that it can be done if I modify the field NRST_MODE to 2 and I really do this. But it doesn't work.The mcu still reset when PG10-NRST comes a low level.

Here is my code in main() to config field NRST_MODE: HAL_FLASH_Unlock(); HAL_FLASH_OB_Unlock(); gFlashOBST.OptionType = OPTIONBYTE_USER; gFlashOBST.USERType  = OB_USER_NRST_MODE; gFlashOBST.USERConfig = FLASH_OPTR_NRST_MODE_1; HAL_FLASHEx_OBProgram(&...

fhu.11 by Associate II
  • 3623 Views
  • 7 replies
  • 0 kudos

FDCAN2 4 times slower than FDCAN1 on STM32G491

I was finally able to find the correct settings to configure my CAN peripherals with correct bitrate after tweaking for a while in STM32CubeMX. The settings that work do not make sense. FDCAN2 is 4 times slower so I had to make clock divider for FDCA...

Resolved! PWM Output Not Generating Waveform for STM32F429ZI

Hi everyone, I'm just trying to test and verify some clock frequencies for a PWM waveform are correct. I used CubeMX to generate some code that has set the clock frequency of the MCU to 72 mHz and I am trying to achieve a 20 kHz PWM frequency. I enab...

EGold.3 by Associate II
  • 3816 Views
  • 6 replies
  • 0 kudos

Sharable D1 SRAMs in the more recent H7 chips

As per RM0468, STM32H72x and STM32H73x chips have 192 KB of SRAM in the D1 domain that is 'sharable' between ITCM and AXI SRAM, ie. it can be allocated as ITCM or AXI SRAM with 64KB granularity,It is known that SRAMs in D1 (or any other domain for th...

HWidj.2 by Associate III
  • 1181 Views
  • 1 replies
  • 0 kudos

Resolved! Setting up RTCC with LSE 32.768kHz Crystal

Hardware 1: STM32F767ZGT6 with LSE Crystal Model:  CM9V-T1A-32.768KHZ-7PF-20PPM-TA-QC Maker: Micro Crystal AG Hardware 2: STM32F767IIT6 with LSE Crystal  Model: ECS-.327-12.5-12R-C-TR Maker: ECS IncCompiler: IAR Workbench v8.32.1Driver: STM32Cube_FW_...

0693W00000Hr4CeQAJ.png

Resolved! How do you know the data transferred from Memory into peripheral has been fully sent VIA DMA into the real world.

I've always been curious to know if there was a method to find out the data transferred via the DMA into the peripheral has been sent out probably. For example a TimerAll it does isCreate an array with varying CCR1 values (Duty Cycles) Once done, ena...

CLeo.1 by Senior II
  • 3200 Views
  • 4 replies
  • 0 kudos

Multiple Interrupts are not working

Hi ,I am working on STM32L0 series controller that has 3 different external interrupts configured on PB11(sensor A),PB2(Sensor B) and PC1(Sensor C).Peripheral connected to PB11 generates interrupt at 1ms interval and PB2 generates interrupt when dat...

BChav.1 by Associate III
  • 1373 Views
  • 2 replies
  • 0 kudos