cancel
Showing results for 
Search instead for 
Did you mean: 

external QSPI flash issue

Nredd.1
Associate III

we are using stm32h745 chip,we want to 64 mb algorthim but in dfp file has 128 mb algorthim only,Controller how to accesess through 64 mb qspi flash.

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Imen.D
ST Employee

Hello @Nredd.1​ ,

Can you please clarify your issue and provide more details ?

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

DFP file?

Which QSPI chip are you using?

Which pins does the QSPI chip use?

What tool chain are you using? Keil?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Hi,
We are using STM32h745XI board with external memory. But the DISCO board has two QSPI flash 64MB each and total of 128MB. Where as in our custom board we used only one chip as 64MB.
But in the project file there is no flash algorithm file for 64MB only 128 MB with 745I-DISCO board is available.
Can you provide flash algorithm for 64MB of STM32H745 Disco project.
Regards,
narendar

Posted the last update on Sunday, tested on the H745XI-DISCO using a single-up configuration

https://github.com/cturvey/stm32extldr/raw/main/h7_mt25ql512a/CLIVEONE-MT25QL512A_STM32H7XX-PF10-PG6-PD11-PF9-PF7-PF6.flm

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nredd.1
Associate III

Hi,

know I am using micron technology qspi flash ic is MT25QL256ABA8ESF-0AAT TR mi,

I am Looking for a Keil .FLM for these pins,

CLK PF10

NCS PG6

D0 PD11

D1 PF9

D2 PF7

D3 PF6

Thanks,

Narendar.

Please contribute via PayPal, or send me a board

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..