STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2S Master has Full Duplex DMA L/R Swapped after Restart

Posted on January 02, 2018 at 22:53I have an application using an STM32F429ZI processor and I'm seeing a strange problem where the L/R audio output gets swapped after changing I2S frequencies.My procedure to change frequencies is as follows:HAL_I2S_...

Showing date and time of file creation in sd card

HelloI have interfaced sd card with controller STM32F779BIi have write text file in sd card but i could not see at what time file is written to sd card doesn't show in properties of that text fileis this is possible , if yes then how can i do that ?B...

Resolved! I think stlink doesn't initialize itself in the nucleo-f767zi

I have a nucleo-f767zi. When I connect it to my Linux computer by USB cable, LD4 keeps blinking red slowly and LD6 goes to solid green. And it stays there forever. I checked in the document LD4 should go to blinking red quickly then solid red. Can yo...

YoungKim by Associate III
  • 1705 Views
  • 2 replies
  • 0 kudos

ADC and DMA Discovery Board F412 - cant get it to work

Hi all,I have two pins where I want to read in the voltage with ADC: PA5 and PA7.Reading in each at its own with polling works fine.Now I want to read them in both and continously. I understand that the right way to go is DMA, contonious mode and sca...

SSchu.4 by Associate II
  • 2330 Views
  • 3 replies
  • 0 kudos