User Activity

Hello to everyone,There are many examples that come with the STM32WL55. Especially LoraWAN examples are very useful. All examples are made to work with TCXO and are not very obvious to those working with XO in code.We made a board with the STM32WL55C...
Hi there,I am trying to compile the SBSFU_2_Images_DualCore project.Although I did it in the correct order according to the document "Getting started with the SBSFU of STM32CubeWL (UM2767)". I am getting a compiler error. I'm sure that, compiling the...
Hello,I am working on a project using STM32Cube_FW_WL_V1.0.0.I cannot compile the 1_Image_SECoreBin project included in the BFU_1_Image sample project.I am using STM32CubeIde on macOS Catalina.I have also read these manuals."Getting started with the ...
We designed a very basic circuit to test an idea. We chose STM32L071K8U6. Because, It met our needs well. Schema  MCU PinmapMCU Clock config in STM32CubeIde  If you look at the clock settings, this processor does not use an external resonator. It cur...