STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L476RG VREF 2.5V to AD?

VREFBUF_TypeDef adRef; adRef.CSR |= VREFBUF_CSR_ENVR | VREFBUF_CSR_VRS; adRef.CSR &= ~VREFBUF_CSR_HIZ;Can someone tell me why I cannot set the AD VREF+ to 2.5V?

0693W00000Ka9K7QAJ.png
SWenn.1 by Senior III
  • 1471 Views
  • 2 replies
  • 0 kudos

Resolved! Trigger ADC1 conversion using TIM3 using registers

Hello,I am trying to have analog voltage converted every 2 seconds using the TRGO signal from TIM3. Without much success. For now, I managed to generate interrupt of TIM3 and in TIM3 Handler to use software trigger for ADC. Here is the code:TIM3:void...

UMilo.1 by Associate III
  • 2520 Views
  • 9 replies
  • 0 kudos

[SOLVED] Issue with custom External Loader for IS25LP256D on STM32F746 - update to V2.5.0 & deinit qspi in Init()

I've made a custom external loader for IS25LP256D on STM32F746. It works well in general except for one problem. Verify doesn't stop when "Verify Programming" is checked. Memory-mapped mode works well, which means reading is good. Erase() and Write()...

External loader for external SDRAM

HelloI want to download my code in the external SDRAM connected to a STM32H743 for debugging purpose. I use the STM32CubeIDE, I wrote an external loader .stldr to configure the FMC.In the debugger tab, I selected the external Loader but it fails to l...

GLeco.1 by Associate
  • 1258 Views
  • 1 replies
  • 0 kudos

STM32G option bytes modification fails in DFU mode

I'm working with a host PC running a C++ Visual Studio project which is running some API calls to implement the DFU protocol. Those API are exposed by some DLL and LIB file available with STM32CubeProgrammer. The host PC is connected via a USB cable...

FValm.1 by Associate III
  • 2243 Views
  • 1 replies
  • 0 kudos

How Can I measure the input frequency by Timer Input Capture?

Hi I measure the frequency from sensor using the Timer Input Capture mode. I set the timer can read minimum 1Hz.72M / 7200/65535 = 0.15HzThis is my code. void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) { HAL_GPIO_WritePin(LED_PORT, IN_LED_...

0693W00000Ka2LTQAZ.png 0693W00000Ka2MkQAJ.png
dKim.1 by Associate II
  • 1109 Views
  • 0 replies
  • 0 kudos