STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[SOLVED] Issue with custom External Loader for IS25LP256D on STM32F746 - update to V2.5.0 & deinit qspi in Init()

I've made a custom external loader for IS25LP256D on STM32F746. It works well in general except for one problem. Verify doesn't stop when "Verify Programming" is checked. Memory-mapped mode works well, which means reading is good. Erase() and Write()...

External loader for external SDRAM

HelloI want to download my code in the external SDRAM connected to a STM32H743 for debugging purpose. I use the STM32CubeIDE, I wrote an external loader .stldr to configure the FMC.In the debugger tab, I selected the external Loader but it fails to l...

GLeco.1 by Associate
  • 1282 Views
  • 1 replies
  • 0 kudos

STM32G option bytes modification fails in DFU mode

I'm working with a host PC running a C++ Visual Studio project which is running some API calls to implement the DFU protocol. Those API are exposed by some DLL and LIB file available with STM32CubeProgrammer. The host PC is connected via a USB cable...

FValm.1 by Associate III
  • 2258 Views
  • 1 replies
  • 0 kudos

How Can I measure the input frequency by Timer Input Capture?

Hi I measure the frequency from sensor using the Timer Input Capture mode. I set the timer can read minimum 1Hz.72M / 7200/65535 = 0.15HzThis is my code. void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) { HAL_GPIO_WritePin(LED_PORT, IN_LED_...

0693W00000Ka2LTQAZ.png 0693W00000Ka2MkQAJ.png
dKim.1 by Associate II
  • 1116 Views
  • 0 replies
  • 0 kudos

STM32G474QB STM32G474QC flash organization

I'm trying to understand how flash memory is organized for STMN32G474QB or STM32G474QC flash. I don't have the micros till now so I cannot do any test to understand that. From the RM0440 manual it seems both are in category 3 device. But when I look ...

0693W00000KZtUHQA1.png
FValm.1 by Associate III
  • 2704 Views
  • 4 replies
  • 0 kudos

sample rate using DMA, ADC and Timer

Hi, I need to sample a signal at a frequency of 10kHz. To avoid the use of the microprocessor I thought of doing it using a 10kHz Timer that triggers the ADC conversion on its falling edge, in addition, I need the ADC read value to be transferred via...

LSoll.1 by Associate II
  • 4583 Views
  • 7 replies
  • 0 kudos