STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L433 Delay before Timer DMA starts

I am having a problem using Timer1 DMA to create a waveform used by one of our peripherals. I have set the timer to count up to 65K with a 1uS tick, and channel 4 as a comparator with a toggle output.I am generating the time between pulses in a tabl...

JMala.3 by Associate III
  • 1561 Views
  • 2 replies
  • 0 kudos

How to connect STM32F411CEU6 to FT232RL USB to TTL

Hi, I'm trying to connect my STM32F411CEU6 to my laptop by using USB to TTL. The USB to TTL I use is FTDI FT232RL module, and I connect my STM to my FT232RL like these following (FT232RL -> STM32):VCC -> 5VGND -> GNDTX -> PB7RX -> PB6Then, I connect...

0693W00000NqOs8QAF.png 0693W00000NqOsDQAV.png
WRama.1 by Associate II
  • 10501 Views
  • 6 replies
  • 0 kudos

Placement of functions in CCMRAM

Hello, i work with STM32F407ZG MCU, i need to place functions in RAM and CCMRAM sections. Placement of functions in RAM is correct, but they take longer than in flash. If I place functions in CCMRAM, then when I call the function, I get an error Hard...

DPavl.11 by Associate II
  • 2347 Views
  • 4 replies
  • 0 kudos

Resolved! What are the differences between STM32L5 and U5 PKA?

Even though it is not really advertised as having changed a lot, it looks like the U5 increased the throughput of the PKA unit nearly 3 fold (upper L5, lower U5):Is this really the case or did the way of obtaining those numbers change in between (e.g...

0693W00000NpQq7QAF.png
OliM by Senior II
  • 2845 Views
  • 4 replies
  • 1 kudos

Resolved! Input capture without HAL with nucleo STM32g474RE

Hello,I would like to measure the period of a square wave (around 1 kHz) with a timer in input capture configuration. I am using TIM5_CH3 on pin PA2 (nucleo G474RE).I would like to receive a bit of help in debugging my code since i am not able to mea...

0693W00000Nq2E1QAJ.png 0693W00000Nq2EGQAZ.png
Tommino by Senior
  • 3258 Views
  • 11 replies
  • 0 kudos

Resolved! how to receive DMA from multiple UART

Hi, I am a newbie in stm32. I am trying to receive DMA from USART1,USART2,USART3.But I am confused as how to do it because, all of them go inside same routine of DMA. Therefore how do I distinguish between different usart. my controller is stm32f103c...

HZaib.1 by Associate III
  • 2021 Views
  • 2 replies
  • 0 kudos