Skip to main content
SGasp.1
Associate III
November 22, 2021
Question

J link plus programming STm32F46

  • November 22, 2021
  • 2 replies
  • 629 views

Hi forum ,

we decided to make a test buying a segger j link plus debug probe.

We are using SWD debug interface

We are using STCubeIde for programming

When w etry to program the micro we got :

- Can not attach to CPU. Trying connect under reset. -

Connecting to CPU via connect under reset failed. 

Any idea what could be ?

Thanks a ot

This topic has been closed for replies.

2 replies

Uwe Bonnes
Chief
November 22, 2021

Double check setup, wiring and voltage levels. 99.9(+ many 9s)% the error is on your side.

Tesla DeLorean
Guru
November 22, 2021

You seem to be having a lot of problems with this board/design.

How exactly are things wired up? Does NRST connect to the debugger interface?

What is the code on your device doing with respect to pins used by the debugger, or putting the processor in low power modes?

Does it program when blank?

Does it program when BOOT0 HIGH?

>>Any idea what could be ?

This really shouldn't need to be a guessing game.

Make a more thorough presentation of the problem, benefits here are two fold, a) it makes you understand/explain what you're doing and how you've tested it, which might cause you to discover the issue, and b) others might be able to see or diagnose what's wrong in the process, without needing to repeat things you've effectively tested already.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..