STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DFU bootloader issues

I am trying to use the built-in bootloader in DFU mode on STM32H743IIT.1. I built my application and created a *.dfu file2. The bootloader starts fine and my device enumerates properly as "STM Device in DFU Mode"3. DfuSe Demo (v3.0.6) detects my devi...

BKlus.1 by Associate III
  • 2091 Views
  • 3 replies
  • 0 kudos

make[1]: *** [Drivers/STM32F1xx_HAL_Driver/Src/subdir.mk:58: Drivers/STM32F1xx_HAL_Driver/Src/stm32f1xx_hal_dma.o] Error 1

I've trying to implement a code for distance sensor AFBR-S50MV85G-EK, but instead of STM32F401RE wich is the mcu recomended by the programing guide I'm using STM32F103C8T6. Now I'm getting the following on console:make -j4 all arm-none-eabi-gcc "../D...

GOrne.1 by Associate
  • 2024 Views
  • 0 replies
  • 0 kudos

Ideas to revive stm32f401re board?

I have a problem with Nucleo STM32F401RE board. For unknown reason the board stopped communicating with PC in debug modes, STM32CubeProgrammer, giving the errors such as: "Error: No STM32 target found!". The PC recognizes the board when connected, ho...

plate30 by Associate II
  • 3119 Views
  • 6 replies
  • 0 kudos

What is the code compatibility on the STM32G4xx series?

If I develop an application for the STM32G431VB for instance, could I drop in a different part in the series with the same footprint and equal or better feature set without retargeting/rebuilding the program? If not, would this work if I stay in the ...

BHall.2 by Associate
  • 1273 Views
  • 2 replies
  • 0 kudos