STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

External Power supply for STEVAL-STWINKT1B

I wanted to know if there was any external power supply available to power the  STEVAL-STWINKT1B board instead of giving it power through the laptop or the provided battery pack. I wanted to implement it in an industrial setup and keep it on for the ...

RMhap.1 by Associate II
  • 2091 Views
  • 3 replies
  • 0 kudos

Facing trouble with SMBUS RX interrupt on STM32L4R9ZI.

Hello, I am facing a strange issue. I have a SMBUS battery and a LTC4100 battery charger chip connected to the micro controllers I2C1 configured as SMBUS. The charger has address 0x12 and the battery has 0x16. All communication is going correctly and...

Makarand by Associate II
  • 870 Views
  • 0 replies
  • 0 kudos

Stack Memory start address

HI All,How to test Stack Over flow in Keil (STM32L0)Is there any document ? or any process to test Stack over flow

VChau by Associate II
  • 2561 Views
  • 3 replies
  • 0 kudos

How to keep program in flash memory

I am trying to use STEVAL-STWINKT1B for predictive maintenance application as an standalone device using Battery pack provided in the kit. But i need to flash the program everytime i remove the battery. I wanted to know if there is a way to keep it w...

RMhap.1 by Associate II
  • 2078 Views
  • 4 replies
  • 0 kudos

STM32L462 configured to wake up from stop mode 2, using RXNE interrupt, not able to receive asynchronous responses sent from the modem.

STM32L462 is configured to wake up from stop 2 mode on RXNE interrupt. Since the response length is unknown and dynamic, have configured interrupt on every character till the end of character is received. MCU is successfully waking up on UART recepti...

KK.4 by Associate II
  • 1055 Views
  • 1 replies
  • 0 kudos