User Activity

Hello,I am using a TESEO LIV3F which supply pins are connected as follow :- Pin 8 (VCC) : 2.4v supplied by a SMPS that may be turned OFF- Pin 7 (VCC IO) : 3.2v supplied by a LDO that may be turned OFF- Pin 6 (Vbatt) : Permanent 3.2v provided by batte...
Hello,I have assembled a PCB that contains a TESEO LIV3F + LNA + SAW, this part of the schematics is shown below.Using the teseo suite pro, the GPS receives no signal so I used a -9dB 1575MHz RF source on the input and measured the RF power at the ou...
Hello everybody,Im am currently trying to connect a STM32H753 to a AD7606B using the parallel interface (FMC) and got it working at some point where the CPU can read/write the data from/to the FMC but it needs a __DSB() before starting to use the rea...
Hello,I would like to use 2x AD7606 for simultaneous sampling of 8 channels, the samples shall be sent to the STM32H753 CPU that will perform some DSP calculations. This system is intended for 3-phase grid monitoring system.I preferred the SPI mode r...
Hello,After updating STM32CubeIDE to version 1.16, starting a debugging session doesn't load program into the STM32L5 target and jumps directly to the reset Handler.I tried programming the bin file using STM32CubeProgrammer and it works well.However,...
Kudos given to