Hi TDK,Thank you for response.I want to verify the system clock running frequency of STM32H7B3 MCU (It support up to 280MHz). For example, If we configured SYSCLK is 256MHz in STM32CubeMx Software. How we can ensure the MCU is running at 256MHz clock...
As per Data Sheet, (DS13195 or STM32H7AxI/G datasheet)Direct channels are connected to analog I/Os (PA0_C, PA1_C, PC2_C and PC3_C)Fast channels correspond for ADCx_INPx to PA6, PB1, PC4, PF11, PF13 and for ADCx_INNx to PA7, PB0,PC5, PF12, PF14I could...
Hi,I already studied this application note. But they said to refer the datasheet for Direct, Fast and Channel Configuration. Based on the STM32H7A3 datasheet, I got the maximum speed for Slow channel is 10MHz.Based on above link application note, the...