STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f7 FMC interfacing external nonmemory chip, like XR16v798

Hi.I`m going to use an octal uart IC named XR16V798 and my MCU is a stm32f756z,I printed my own designed board which connected these two ICs as follows:just to mention, I haven`t used FMC with any other device before, now I dont know how to work with...

0693W00000UnuCVQAZ.png
HSh..2 by Associate II
  • 2161 Views
  • 4 replies
  • 1 kudos

Software reset issue

1. HAL_NVIC_SystemReset() does not work. it always stays at __NOP(), no reset  for(;;)                              /* wait until reset */ {  __NOP(); }2. Before I implemented ADC with DMA, the soft reset below works. But after implemented ADC with D...

DMA memory to memory doesn't work

Hi guys im doing a simple 5 byte memory to memory dma transfer with timer update request.As stm32f407 reference manual said timer8 update is connected to dma2 stream 1.Here is the timer config by cube.And the dma cube config:I started the dma and exp...

0693W00000Uo7PIQAZ.png 0693W00000Uo7PSQAZ.png 0693W00000Uo7PXQAZ.png 0693W00000Uo7PrQAJ.png

STM32L432 and STM32H745 DAC in DMA mode has shifted data output

Hi, I have a problem with DAC output, same problem with STM32L4 and STM32H7. I have to continuously output a step wave (3 levels), for this purpose I use a Timer and DMA in circular mode to output an array of 3 values.The code is very simple, I use a...

0693W00000Uo1oqQAB.png
GMG by Associate III
  • 1427 Views
  • 1 replies
  • 0 kudos

Resolved! How DMA works when is triggered with events?

Hello guys.Im a little confused about dma functionality.My question is that if dma controller can start a peripheral or it just can move data from the peripheral to memory.For example when using adc with dma:Is it dma that start the conversion and mo...