STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 for medical use.

We need STM32 MCU types for use in medical instruments. Does ST have Medical grade STM32 MCU's? It must be recommended for new design with long life time.

MCUpwr by Associate III
  • 1596 Views
  • 2 replies
  • 0 kudos

Hi all, I am back with another problem!! I am using timer 2 in 103C8 controller for 0.1 Sec time delay. However, it is generating 5 times the calculated delay. My initialization code for this delay is given below. Timer interrupt is enabled.

htim2.Init.Prescaler = 1000;htim2.Init.CounterMode = TIM_COUNTERMODE_UP;htim2.Init.Period = 7200;htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;However if I change the prescaler to 200, ...

Nucleo-L432KC program not starting

Hello, I'm new on this forum.Last time I bought Nucleo-L432KC board. I have very strange issue with flashing binary. I created simple project in STM32CubeMX for blinking LED every 1 second. I use this command to flash:st-flash --reset write blink.bin...

DD.14 by Associate II
  • 3580 Views
  • 6 replies
  • 0 kudos

I am having difficulty receiving data on USART2. It is receiving one character when I use HAL_UART_Receive_IT interrupts. I am trying to receive some characters from ADUCM360 USART.

I can see transmitting characters from ADUCM360 to STM32.But it does not capture the incoming characters from STM32 using interrupts. Any help on this very much appreciated. Thank you

cjaya.1 by Associate II
  • 5967 Views
  • 18 replies
  • 0 kudos

Resolved! Can the STM32L4 transmit and receive USART over DMA?

Hello, I am inquiring about USART communication using DMA. I am following github.com/MaJerle/stm32-usart-uart-dma-rx-tx tutorial using the low level drivers for a STM32L432. I have reception working with no troubles and I believe my interrupts are be...

ABicc.1 by Associate
  • 2591 Views
  • 1 replies
  • 0 kudos

I am trying to read 3 ADC channels via DMA. One weird thing happen: if I use a breakpoint on the line of the readings, I get the correct values from the ADC. If I don't use a breakpoint, the values are always 0 or random. Can you help me ?

I tried using delays, but they don't solve the problem. Data are retrieved using HAL_ADC_Start_DMA(&hadc1, value, DATA_LENGTH) HAL_ADC_Stop_DMA(&hadc1);here below my intialization and function:void MX_ADC1_Init(void){    ADC_ChannelConfTypeDef sConf...

LScar.1 by Associate
  • 1250 Views
  • 1 replies
  • 0 kudos