Skip to main content
JKaz.1
Associate III
April 20, 2022
Question

How to program the Option Bytes on a G0?

  • April 20, 2022
  • 2 replies
  • 1445 views

I'm trying to program the option bytes on an STM32G0B1 but it keeps timing out at the end of the program sequence and never actually succeeds, no matter how many times I try.

I enable the Flash peripheral

I (successfully) unlock the flash

I (successfully) unlock the option bytes

I program the option bytes

... and it times out 10 times

then it calls OB_Launch and hard faults.

.. what am I missing? This was easy on the H7...

{	
	__HAL_RCC_FLASH_CLK_ENABLE();
 
	FLASH_OBProgramInitTypeDef flashDef;
	memset(&flashDef, 0, sizeof(FLASH_OBProgramInitTypeDef));	
	HAL_FLASHEx_OBGetConfig(&flashDef);
	
	if ((flashDef.USERConfig & OB_BOR_ENABLE) == 0)
	{
		for (int i = 0; i < 10; i++)
		{
			if (HAL_FLASH_Unlock() == HAL_OK)
				break;
		}		
		
		for (int i = 0; i < 10; i++)
		{
			if (HAL_FLASH_OB_Unlock() == HAL_OK)
				break;
		}	
	
		memset(&flashDef, 0, sizeof(FLASH_OBProgramInitTypeDef));
		flashDef.OptionType = OPTIONBYTE_USER;
		flashDef.USERType = OB_USER_BOR_EN;
		flashDef.USERConfig = OB_BOR_ENABLE;
	
		for (int i = 0; i < 10; i++)
		{
			if (HAL_FLASHEx_OBProgram(&flashDef) == HAL_OK)
				break;
		}
		
		HAL_FLASH_OB_Launch();
	
		for (int i = 0; i < 10; i++)
		{
			if (HAL_FLASH_OB_Lock() == HAL_OK)
				break;
		}
	
		for (int i = 0; i < 10; i++)
		{
			if (HAL_FLASH_Lock() == HAL_OK)
				break;
		}
	}
}

This topic has been closed for replies.

2 replies

Pavel A.
April 20, 2022

Same thing as here?

JKaz.1
JKaz.1Author
Associate III
April 20, 2022

Yup, looks like it. I didn't find that post while searching the forums to see if anyone had similar difficulties... Kinda surprised this doesn't have an answer yet...