STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flash Programming Error Even if Flash was erased.

Hi guys,I am using and STM32L552ZET6 and I get a behavior I can not exaplain. The device is power at 1.8V in case it matters. So to put it shortly I have 2 blocks of 8 pages each. At first start I erase both of the blocks and write only in block 1 so...

CDan.1 by Associate II
  • 3903 Views
  • 3 replies
  • 0 kudos

CPU test bug in the X-CUBE-STL (gcc)

Hi, this isn't really a question, but I figured I'd share back with the community (and hopefully bring the change back into ST's next release) on the X-CUBE-STL CPU test code.There are some instances, where the APSR has some bit set in what ARM docum...

TK.0 by Associate
  • 1953 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F429ZI interface to GEN4-FT813-CTP-CLB:

Everyone, Posting for the first time here. We've been working with a 4d display that's based on an FT813 IC. The issue that we came to so far is the following.0x7C during Initialization is never detected although, it is detected from MISO. This is re...

0693W00000HnkROQAZ.png

STM32H743XIH6 芯片背�?�有水�?�,有划痕,请问是原厂工艺问题导致的�?�? 是原厂出厂就存在的�?�?

STM32H743XIH6  芯片背�?�有水�?�,有划痕,请问是原厂工艺问题导致的�?�? 是原厂出厂就存在的�?�?平时是真空�?存的,今天拆包�?��?�现有上�?�两�?情况,请帮忙解答�?

0693W00000WINQ1QAP.jpg 0693W00000WINQaQAP.png
满陈.1 by Associate
  • 918 Views
  • 1 replies
  • 0 kudos

How to manage 2 channel PWM with DMA - STM32L073

We try to generate audio signal with 2 PWM signals. We use TIM2_CH1 and TIM2_CH2 with DMA1 channel 5 and channel 3. This two PWM signals must be synchronized, but we noticed some delay between this 2 channels, which unfortunately is not constant. For...

mrasz.1 by Associate
  • 1305 Views
  • 1 replies
  • 0 kudos

In Rx Polling Mode, HAL_UART_Receive() is stuck in UART_WaitOnFlagUntilTimeout() waiting for the RXNE flag to get set in the UART's Status Register.

I'm using a STM32F407-Disc1 board, and my polled HAL_UART_Receive() is stuck waiting for the RXNE flag to get set in the UART Status register. Ironically, when using the STM32CubeIDE debugger and looking at the SFR registers for my UART, it looks li...

RJepp.1 by Associate II
  • 1636 Views
  • 2 replies
  • 0 kudos

STM32U5 ADC internal channel

Hello,I'm facing some issues sampling ADC internal channel in of STM32u575.In particular these are the steps I'm following:VDDA enableADC Clock ConfigurationHAL_ADC_Init (&ADC_Handle[i])Interrupt configuration.Then, I configure the ADC channel to rea...

Resolved! VREFINT - sporadic false(?) readings

Using a STM32F091 board, I set up the ADC to:sample at the longest selectable sampling time (239.5 cycles)clock source is the internal 14 MHz RC oscresolution 12 bitsequence of all available channels incl. vrefintAt startup, there is a slight deviati...

SKled.1 by Senior II
  • 3844 Views
  • 6 replies
  • 1 kudos

STM32U5 controller RTC accuracy

Hi,I am trying to enable RTC functionality in Nucleo STM32U575ZI board. As one of my requirement I wanted to understand how much accuracy we can get for STM32U5 controller ? Any documentation or suggestion would help a lot.Thanks!!

NM.1 by Associate II
  • 1575 Views
  • 2 replies
  • 0 kudos