User Activity

Hi, I have an FPGA connected to the STM32 (STM32F746IGT). The FPGA is set up to work as SRAM (tested and confirmed working). I’m using the STM’s Flexible Memory Controller to read from the ‘sram’. Now this works, but after 2 read cycles, the FMC stop...
Hi all, I've been trying to use the virtual com port on the "STM32F4DISCOVERY" with no luck. My current IDE is STM32CubeIDE v1.3.1, STM32CubeMx v5.6.1, I'm also using firmware pack FW_F4 V1.25.0.Ive started a brand new project, used the CubeIDE board...