STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Which OCTOSPI pins can be used as MOSI and MISO in single mode?

It is written in the STM32U575/585 reference manual (see below) that the data is sent to the external device over the SO(IO0) signal and that The data received from the external device arrives via SI(IO1). Now, SO is known as Slave Out but here it i...

0693W00000Y8IX0QAN.png
bmn by Associate II
  • 3196 Views
  • 2 replies
  • 0 kudos

I2S clock strobing

The stm32u5xx_hal_sai.c sets up the I2S clock strobing like this:static HAL_StatusTypeDef SAI_InitI2S(SAI_HandleTypeDef *hsai, uint32_t protocol, uint32_t datasize, uint32_t nbslot) { HAL_StatusTypeDef status = HAL_OK;   hsai->Init.Protocol ...

clock setting, STM32H750

Hello,I have two different clock setting and only one of them works - but I have no idea why?The only difference is the PLLM and PLLN value: RCC_OscInitStruct.PLL.PLLM = 25; // 5 NOT OK RCC_OscInitStruct.PLL.PLLN = 432; // 160 NOT OKWould appreciate ...

pk84 by Senior
  • 6366 Views
  • 11 replies
  • 0 kudos

FW upgrade via DFU

I am trying to upgrade my uC via dfu-util however i receive an error and i do not know how could i debug it dfu-util: Error during download get_statusdfu-util 0.9Opening DFU capable USB device...ID 0483:df11Run-time device DFU version 011aClaiming US...

EPop.2 by Associate II
  • 2721 Views
  • 2 replies
  • 0 kudos

STM32G431 Break input for PWMs

I am generating two PWMs with TIM1 CH1 and CH2 .I want to stop the PWMs when Break input is present. I have configured the STM32 Break input in the STM32cubeIDE and able to stop the PWMs when Break input is HIGH(3.3v).I needed the reverse way now lik...

sshan.2 by Associate III
  • 2946 Views
  • 4 replies
  • 1 kudos

Is there any way to "pace" bytes in an I2C transmission?

Hi,I am interfacing to a TI device that requires a 100us delay between each I2C byte and I can't think of any way that doesn't involve "hacking", i.e. using timer delays, interrupts, etc. Is there a more elegant way to do it using the ST I2C implemen...

GoEk by Associate III
  • 5525 Views
  • 13 replies
  • 1 kudos