User Activity

I ran into a small footnote in AN3155 stating "System reset is called only for some STM32 BL (STM32F0/F2/F4/F7) and some STM32L4 (STM32L412xx/422xx, STM32L43xxx/44xxx, STM32L45xxx/46xxx) products."Now I run into the problem that after flashing the fi...
Hi,I have a product which runs an application that uses SBSFU on a STM32. The product is battery powered by a small battery. After the small battery is almost depleted, it charges itself by drawing power from a larger external battery. If however tha...
@Jocelyn RICARD​ I've built, installed and used SBSFU to successfully update the firmware through the serial terminal with a YModem transfer. This update was from version "0" to version "1". Now I have built a new version "2" which only differs from ...
I am using the KMS of SBSFU to store my TLS certificates during the provisioning process. When I flash a new user firmware application the certificates inside the KMS are deleted too. So each time I want to run new user firmware, I have to go through...
I have an undefined reference error to several secure engine functions, for example SE_APP_GetActiveFwStateI have read this thread:https://community.st.com/s/question/0D53W000017PGUKSA4/how-to-call-secureengine-functions-from-my-applicationAnd what I...